<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6 SoloX Cortex-M4 QSPI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SoloX-Cortex-M4-QSPI/m-p/457670#M71578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to make read, write and erase functions for QSPI on iMX6 SoloX SabreSD board with QSPI NOR Micron n25q256.&lt;/P&gt;&lt;P&gt;Are there any resources with examples on how to read, write or erase from Cortex-M4? &lt;/P&gt;&lt;P&gt;I'm using bare-metal c. Current code runs from RAM and does not use QSPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX 4.1 for imx6sx does not have qspi example. If there is one, it could help a lot.&lt;/P&gt;&lt;P&gt;uBoot for Cortex-A9 has the sf command. This code could maybe be used and rewritten for Cortex-M4.&lt;/P&gt;&lt;P&gt;MQX 4.2, which does not support imx6sx, has the qspi example which could also maybe be rewritten.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone give me advice which way to go?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Nov 2015 12:43:23 GMT</pubDate>
    <dc:creator>zvonimirmandi_</dc:creator>
    <dc:date>2015-11-05T12:43:23Z</dc:date>
    <item>
      <title>iMX6 SoloX Cortex-M4 QSPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SoloX-Cortex-M4-QSPI/m-p/457670#M71578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to make read, write and erase functions for QSPI on iMX6 SoloX SabreSD board with QSPI NOR Micron n25q256.&lt;/P&gt;&lt;P&gt;Are there any resources with examples on how to read, write or erase from Cortex-M4? &lt;/P&gt;&lt;P&gt;I'm using bare-metal c. Current code runs from RAM and does not use QSPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX 4.1 for imx6sx does not have qspi example. If there is one, it could help a lot.&lt;/P&gt;&lt;P&gt;uBoot for Cortex-A9 has the sf command. This code could maybe be used and rewritten for Cortex-M4.&lt;/P&gt;&lt;P&gt;MQX 4.2, which does not support imx6sx, has the qspi example which could also maybe be rewritten.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone give me advice which way to go?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Nov 2015 12:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SoloX-Cortex-M4-QSPI/m-p/457670#M71578</guid>
      <dc:creator>zvonimirmandi_</dc:creator>
      <dc:date>2015-11-05T12:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SoloX Cortex-M4 QSPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SoloX-Cortex-M4-QSPI/m-p/457671#M71579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could refer to the following document from the Community, which explains how to generate, download and run an application on the M4 core of the i.MX6SX:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-106148"&gt;Customizing MQX applications on i.MX6SX.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Nov 2015 20:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SoloX-Cortex-M4-QSPI/m-p/457671#M71579</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-11-09T20:58:53Z</dc:date>
    </item>
  </channel>
</rss>