<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Dual parallel camera input!!!!</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Dual-parallel-camera-input/m-p/457499#M71526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI chilwonna&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general yes, this may be supported as max. performance is 240MHz per IPU&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52604i7A30DB5B1AC4CC66/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Aug 2015 10:55:19 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-08-21T10:55:19Z</dc:date>
    <item>
      <title>Dual parallel camera input!!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-parallel-camera-input/m-p/457498#M71525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to design with iMX6 dual.&lt;/P&gt;&lt;P&gt;I will connect dual parallel camera.&lt;/P&gt;&lt;P&gt;Cam1 = 1280*720*30fps, YUV -&amp;gt;&amp;nbsp; IPU#1_CSI0&lt;/P&gt;&lt;P&gt;Cam2 = 2560*1920*30fps, mono Bayer -&amp;gt; IPU#2_CSI1&lt;/P&gt;&lt;P&gt;Display = Parallel display port&lt;/P&gt;&lt;P&gt;Board has to capture two camera at same time and&amp;nbsp; diplays with Cam1.&lt;/P&gt;&lt;P&gt;Cam2 has to be saved to memory.&lt;/P&gt;&lt;P&gt;Is it possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 09:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-parallel-camera-input/m-p/457498#M71525</guid>
      <dc:creator>chilwonna</dc:creator>
      <dc:date>2015-08-21T09:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: Dual parallel camera input!!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dual-parallel-camera-input/m-p/457499#M71526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI chilwonna&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general yes, this may be supported as max. performance is 240MHz per IPU&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52604i7A30DB5B1AC4CC66/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 10:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dual-parallel-camera-input/m-p/457499#M71526</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-08-21T10:55:19Z</dc:date>
    </item>
  </channel>
</rss>