<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto connman with wilink8 module problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457061#M71376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ivan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where do you get the wLink8 driver ? for what Kernel version is the driver made for?,&amp;nbsp; what version of BSP are you using and for what I see you are using QT, are you using a freescale board?,&amp;nbsp; We have test the freescale BSP with the Wl12xx driver as you mention also and do not have the problem so I think it is in the way the driver of Wlink8 has been made or requirements for it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Sep 2015 14:40:59 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2015-09-14T14:40:59Z</dc:date>
    <item>
      <title>Yocto connman with wilink8 module problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457060#M71375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone faced the problem with the Yocto network connection manager (connman) and wilink8 (wl18xx wi-fi+bt) module?&lt;/P&gt;&lt;P&gt;The problem is that the connman does not connect to Wi-Fi network with wilink8 module. There are no issue with old wilink6 module (wl12xx).&lt;/P&gt;&lt;P&gt;I do&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;&lt;STRONG&gt;ifconfig wlan0 up&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;&lt;STRONG&gt;iw wlan0 scan&lt;/STRONG&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;successfully in the terminal, but when I press "Enable/Disable" and "Scan" buttons in connman window, nothing happened.&lt;/P&gt;&lt;P&gt;I have installed &lt;STRONG&gt;wpa_supplicant&lt;/STRONG&gt; package.&lt;/P&gt;&lt;P&gt;Connman is in the red circle.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52601i5204CD2F1F2D7292/image-size/large?v=v2&amp;amp;px=999" title="yocto.jpg" alt="yocto.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 07:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457060#M71375</guid>
      <dc:creator>ivannikolaenko</dc:creator>
      <dc:date>2015-08-21T07:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto connman with wilink8 module problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457061#M71376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ivan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where do you get the wLink8 driver ? for what Kernel version is the driver made for?,&amp;nbsp; what version of BSP are you using and for what I see you are using QT, are you using a freescale board?,&amp;nbsp; We have test the freescale BSP with the Wl12xx driver as you mention also and do not have the problem so I think it is in the way the driver of Wlink8 has been made or requirements for it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Sep 2015 14:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457061#M71376</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-09-14T14:40:59Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto connman with wilink8 module problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457062#M71377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello jamesbone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got wilink8 driver source code from git://git.ti.com/wilink8-wlan/build-utilites.git and build it for my&lt;STRONG&gt; 3.10.53 Linux kernel&lt;/STRONG&gt;. I am using latest &lt;STRONG&gt;Fido (1.8) FSL-BSP &lt;/STRONG&gt;with our custom i.MX6Q-based board. &lt;BR /&gt;Could You help me to figure out the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 12:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-connman-with-wilink8-module-problem/m-p/457062#M71377</guid>
      <dc:creator>ivannikolaenko</dc:creator>
      <dc:date>2015-09-17T12:50:04Z</dc:date>
    </item>
  </channel>
</rss>