<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how to copy to flash in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456865#M71338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi thanks for your reply&lt;/P&gt;&lt;P&gt;can you send any doc or pdf which gives procedure for this&lt;/P&gt;&lt;P&gt;this is my new board i am going to use arm ds5&lt;/P&gt;&lt;P&gt;i am following this procedure&lt;/P&gt;&lt;P&gt;1. load u-boot using arm ds-5 and run from ram&lt;/P&gt;&lt;P&gt;2.load u-boot.imx binary in to ram in another location than i will use cp command to write into nor flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is this works ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jul 2015 07:57:23 GMT</pubDate>
    <dc:creator>saida</dc:creator>
    <dc:date>2015-07-07T07:57:23Z</dc:date>
    <item>
      <title>how to copy to flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456862#M71335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&amp;nbsp; i.mx6 community&lt;/P&gt;&lt;P&gt;i have i.mx6 dl sabre board with this reference i made custom board and i am ready to port u-boot which is sabre board's u-boot&lt;/P&gt;&lt;P&gt;can i load u-boot.imx to RAM than copy to NOR FLASH (s29jl064h chip).&lt;/P&gt;&lt;P&gt;how to do this ?&lt;/P&gt;&lt;P&gt;can any one help in this regard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can a&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 05:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456862#M71335</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-07-07T05:28:34Z</dc:date>
    </item>
    <item>
      <title>Re: how to copy to flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456863#M71336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use MFG Tool provided by Freescale. It has support to update firmware on NOR FLASH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 05:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456863#M71336</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2015-07-07T05:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: how to copy to flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456864#M71337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please use the enclosed MFG configuration as an example.&lt;/P&gt;&lt;P&gt;It loads U-boot to i.MX6 DRAM. Than You may use NFS, TFTP,&lt;/P&gt;&lt;P&gt;FAT SD to load and burn any image, assuming U-boot has the &lt;/P&gt;&lt;P&gt;needed drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 06:47:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456864#M71337</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-07-07T06:47:20Z</dc:date>
    </item>
    <item>
      <title>Re: how to copy to flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456865#M71338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi thanks for your reply&lt;/P&gt;&lt;P&gt;can you send any doc or pdf which gives procedure for this&lt;/P&gt;&lt;P&gt;this is my new board i am going to use arm ds5&lt;/P&gt;&lt;P&gt;i am following this procedure&lt;/P&gt;&lt;P&gt;1. load u-boot using arm ds-5 and run from ram&lt;/P&gt;&lt;P&gt;2.load u-boot.imx binary in to ram in another location than i will use cp command to write into nor flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is this works ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 07:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456865#M71338</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-07-07T07:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: how to copy to flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456866#M71339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Saida, hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You may create SR via FSL Web in order to get some recommendations about U-boot &lt;/P&gt;&lt;P&gt;debugging with DS-5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 06:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-copy-to-flash/m-p/456866#M71339</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-07-21T06:52:19Z</dc:date>
    </item>
  </channel>
</rss>