<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックVDDHIGH Voltage Range</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-Voltage-Range/m-p/456423#M71232</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a I.MX 6 SoloX processor with a MMPF0200 PMIC. I would like to use the pre-programmed Device F0. My problem is now, that there is no default voltage which fits the requirements for the VDD_HIGH voltage Domain.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SW1 is used for Core Voltage&lt;/LI&gt;&lt;LI&gt;SW2 should be used for 3.3V Peripheral Interfaces of the i.MX&lt;/LI&gt;&lt;LI&gt;SW3 is used for DDR&lt;/LI&gt;&lt;LI&gt;VGEN1 delivers 1.5V (not in use)&lt;/LI&gt;&lt;LI&gt;VGEN2 delivers 1.5V (not in use)&lt;/LI&gt;&lt;LI&gt;VGEN3 delivers 2.5V and sould bes used for Ethernet logic interface&lt;/LI&gt;&lt;LI&gt;VGEN4 delivers 1.8V and sould bes used for low-power Mode for eMMC interface&lt;/LI&gt;&lt;LI&gt;VGEN5 delivers 2.8V (not in use)&lt;/LI&gt;&lt;LI&gt;VGEN6 delivers 3.3V &lt;EM&gt;VDD_HIGH?&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I am able to use VGEN1,2,5 or 6. The problem is now, that the VDD_HIGH-Domain powers the clock generation. So, the voltage has to be correct at startup an cannot be overwritten in Software. VGEN1&amp;amp;2 can't be used because the voltage would be too low. VGEN5&amp;amp;6 are right on the limits of the recommended power levels. So, if the level would wobble a bit (which they always will) it is possbile that both voltages violate the Voltage contraints. VGEN5 cant be used because the maximum current is a bit too low (100mA when max. 125mA needed, chapter 4.1.5)&lt;/P&gt;&lt;P&gt;But: In the IM.X 6 SoloX Industrial Application Datasheet Chapter 4.1.6 all test cases use 3.3V to Power VDD_HIGH.&lt;/P&gt;&lt;P&gt;So my question is: Is it guaranteed that the Processor will start up if I apply VGEN6 with 3.3V to this Input even if it may be a bit higher?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 06:33:16 GMT</pubDate>
    <dc:creator>DBMicro</dc:creator>
    <dc:date>2015-09-17T06:33:16Z</dc:date>
    <item>
      <title>VDDHIGH Voltage Range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-Voltage-Range/m-p/456423#M71232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a I.MX 6 SoloX processor with a MMPF0200 PMIC. I would like to use the pre-programmed Device F0. My problem is now, that there is no default voltage which fits the requirements for the VDD_HIGH voltage Domain.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SW1 is used for Core Voltage&lt;/LI&gt;&lt;LI&gt;SW2 should be used for 3.3V Peripheral Interfaces of the i.MX&lt;/LI&gt;&lt;LI&gt;SW3 is used for DDR&lt;/LI&gt;&lt;LI&gt;VGEN1 delivers 1.5V (not in use)&lt;/LI&gt;&lt;LI&gt;VGEN2 delivers 1.5V (not in use)&lt;/LI&gt;&lt;LI&gt;VGEN3 delivers 2.5V and sould bes used for Ethernet logic interface&lt;/LI&gt;&lt;LI&gt;VGEN4 delivers 1.8V and sould bes used for low-power Mode for eMMC interface&lt;/LI&gt;&lt;LI&gt;VGEN5 delivers 2.8V (not in use)&lt;/LI&gt;&lt;LI&gt;VGEN6 delivers 3.3V &lt;EM&gt;VDD_HIGH?&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I am able to use VGEN1,2,5 or 6. The problem is now, that the VDD_HIGH-Domain powers the clock generation. So, the voltage has to be correct at startup an cannot be overwritten in Software. VGEN1&amp;amp;2 can't be used because the voltage would be too low. VGEN5&amp;amp;6 are right on the limits of the recommended power levels. So, if the level would wobble a bit (which they always will) it is possbile that both voltages violate the Voltage contraints. VGEN5 cant be used because the maximum current is a bit too low (100mA when max. 125mA needed, chapter 4.1.5)&lt;/P&gt;&lt;P&gt;But: In the IM.X 6 SoloX Industrial Application Datasheet Chapter 4.1.6 all test cases use 3.3V to Power VDD_HIGH.&lt;/P&gt;&lt;P&gt;So my question is: Is it guaranteed that the Processor will start up if I apply VGEN6 with 3.3V to this Input even if it may be a bit higher?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 06:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-Voltage-Range/m-p/456423#M71232</guid>
      <dc:creator>DBMicro</dc:creator>
      <dc:date>2015-09-17T06:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: VDDHIGH Voltage Range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-Voltage-Range/m-p/456424#M71233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi DBMicro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes it will start up, however for longterm reliability it is not recommended to&lt;/P&gt;&lt;P&gt;use higher voltages than recommended by datsheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 08:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VDDHIGH-Voltage-Range/m-p/456424#M71233</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-17T08:17:29Z</dc:date>
    </item>
  </channel>
</rss>