<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 duallite-60FPS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456089#M71187</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Dear all,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;we are using IMX6 Dual processor to run a Full HD Animated image in our TFT.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Now the image Frame rate 30 FPS.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Does our processor have the capability to run the same in 60 FPS?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. In the Datasheet it has mentioned without "Multimedia Framework" the The video can be recorded and the same can be playbacked at 60 FPS.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Kinldy HELP:)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Regards,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Muthuraj M&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;+919003281838&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2015 09:59:36 GMT</pubDate>
    <dc:creator>muthurajm</dc:creator>
    <dc:date>2015-05-22T09:59:36Z</dc:date>
    <item>
      <title>i.MX6 duallite-60FPS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456089#M71187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Dear all,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;we are using IMX6 Dual processor to run a Full HD Animated image in our TFT.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Now the image Frame rate 30 FPS.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Does our processor have the capability to run the same in 60 FPS?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. In the Datasheet it has mentioned without "Multimedia Framework" the The video can be recorded and the same can be playbacked at 60 FPS.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Kinldy HELP:)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Regards,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Muthuraj M&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;+919003281838&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 09:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456089#M71187</guid>
      <dc:creator>muthurajm</dc:creator>
      <dc:date>2015-05-22T09:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 duallite-60FPS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456090#M71188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Muthuraj &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;typical value is 30fps as shown on presentation p.21&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100482"&gt;A Deep Dive into Image Processing for i.MX 6 Series Applications Processors&lt;/A&gt; &lt;/P&gt;&lt;P&gt;p.118 shows 60fps use case.&lt;/P&gt;&lt;P&gt;Performance depends om use case, since some IPU submodules are limited to 1920x1080 @ 30 fps,&lt;/P&gt;&lt;P&gt;sect.38.1.2.1.5.3 Image Converter (IC) &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6SDLRM&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 May 2015 02:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456090#M71188</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-05-25T02:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 duallite-60FPS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456091#M71189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Igor:)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 10:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456091#M71189</guid>
      <dc:creator>muthurajm</dc:creator>
      <dc:date>2015-05-26T10:54:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 duallite-60FPS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456092#M71190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the resolution about &lt;A href="mailto:640x480@60fps,"&gt;640x480&lt;/A&gt;&amp;nbsp;60fps and data format is RGB888 from mipi-csi2, is it possible to preview in 60fps?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jun 2019 04:44:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-duallite-60FPS/m-p/456092#M71190</guid>
      <dc:creator>zhengl</dc:creator>
      <dc:date>2019-06-23T04:44:24Z</dc:date>
    </item>
  </channel>
</rss>