<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTransient in IMX6SL USB causes USB to Fail</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Transient-in-IMX6SL-USB-causes-USB-to-Fail/m-p/455324#M70957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the demo board for the IMX6SL. As a reference for our own board. All the diodes and suppressors are the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we perform a Electrical Fast Transient on the USB cable (feeding into USB_OTG1) the USB port stops performing. The USB controller refuses to hand shake. &lt;/P&gt;&lt;P&gt;Both DP and DN of the USB controller is routed to a: &lt;A href="http://www.semtech.com/circuit-protection/esd-protection/srv05-4/" title="http://www.semtech.com/circuit-protection/esd-protection/srv05-4/"&gt;SRV05-4 RailClamp® Low-Capacitance TVS Diode Array | Semtech&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The processor still works, all other ports work fine. The only issue is no hand shaking with the host over USB. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Has anyone run into this problem? Any help would be appreciated. &lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Apr 2015 19:29:56 GMT</pubDate>
    <dc:creator>jparrish88</dc:creator>
    <dc:date>2015-04-29T19:29:56Z</dc:date>
    <item>
      <title>Transient in IMX6SL USB causes USB to Fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transient-in-IMX6SL-USB-causes-USB-to-Fail/m-p/455324#M70957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the demo board for the IMX6SL. As a reference for our own board. All the diodes and suppressors are the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When we perform a Electrical Fast Transient on the USB cable (feeding into USB_OTG1) the USB port stops performing. The USB controller refuses to hand shake. &lt;/P&gt;&lt;P&gt;Both DP and DN of the USB controller is routed to a: &lt;A href="http://www.semtech.com/circuit-protection/esd-protection/srv05-4/" title="http://www.semtech.com/circuit-protection/esd-protection/srv05-4/"&gt;SRV05-4 RailClamp® Low-Capacitance TVS Diode Array | Semtech&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The processor still works, all other ports work fine. The only issue is no hand shaking with the host over USB. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Has anyone run into this problem? Any help would be appreciated. &lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 19:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transient-in-IMX6SL-USB-causes-USB-to-Fail/m-p/455324#M70957</guid>
      <dc:creator>jparrish88</dc:creator>
      <dc:date>2015-04-29T19:29:56Z</dc:date>
    </item>
    <item>
      <title>Re: Transient in IMX6SL USB causes USB to Fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transient-in-IMX6SL-USB-causes-USB-to-Fail/m-p/455325#M70958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jparrish88&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to analyze errors using&lt;/P&gt;&lt;P&gt;sect.65.4.3.15.1.1 Transaction Error &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;and try to reset (or even reinitialize) USB controller.&lt;/P&gt;&lt;P&gt;Another way - try to add more shielding to design and use&lt;/P&gt;&lt;P&gt;more quality and short usb cable. Also one can try to limit speed&lt;/P&gt;&lt;P&gt;to USB Full or even Low.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2015 04:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transient-in-IMX6SL-USB-causes-USB-to-Fail/m-p/455325#M70958</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-30T04:33:27Z</dc:date>
    </item>
  </channel>
</rss>