<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Hi in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Hi/m-p/455219#M70949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Take a look in variable IMAGE_FEATURES&lt;SPAN class="permalink"&gt; [1]&lt;/SPAN&gt; which possible values are listed in [2]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#usingpoky-extend-customimage-imagefeatures" title="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#usingpoky-extend-customimage-imagefeatures"&gt;[1] Yocto Project Mega-Manual&lt;/A&gt; &lt;/P&gt;&lt;P&gt;[2] &lt;A href="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#var-EXTRA_IMAGE_FEATURES" title="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#var-EXTRA_IMAGE_FEATURES"&gt;Yocto Project Mega-Manual&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the same manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;CODE class="filename"&gt;core-image-minimal&lt;/CODE&gt;: A small image just capable of allowing a device to boot.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Prefer to use core-image-base instead, because minimal is NOT supposed to be full featured image, it's only a bring up image. And add the native features you need, not only *gcc*.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Dec 2015 16:42:37 GMT</pubDate>
    <dc:creator>daiane_angolini</dc:creator>
    <dc:date>2015-12-01T16:42:37Z</dc:date>
    <item>
      <title>Hi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hi/m-p/455218#M70948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am a newbie to yocto. Please help me.&lt;/P&gt;&lt;P&gt;I am trying to add gcc package to my core-image-minimal using IMAGE_INSTALL_append variable in local.conf file, but after bitbake the package is not getting added or installed in the image. &lt;/P&gt;&lt;P&gt;I have initialized the variable as follows in local.conf file.&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " gcc"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then executed bitbake -k core-image-minimal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Dec 2015 13:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hi/m-p/455218#M70948</guid>
      <dc:creator>vikramks1</dc:creator>
      <dc:date>2015-12-01T13:54:00Z</dc:date>
    </item>
    <item>
      <title>Re: Hi</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hi/m-p/455219#M70949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Take a look in variable IMAGE_FEATURES&lt;SPAN class="permalink"&gt; [1]&lt;/SPAN&gt; which possible values are listed in [2]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#usingpoky-extend-customimage-imagefeatures" title="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#usingpoky-extend-customimage-imagefeatures"&gt;[1] Yocto Project Mega-Manual&lt;/A&gt; &lt;/P&gt;&lt;P&gt;[2] &lt;A href="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#var-EXTRA_IMAGE_FEATURES" title="http://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#var-EXTRA_IMAGE_FEATURES"&gt;Yocto Project Mega-Manual&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the same manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;CODE class="filename"&gt;core-image-minimal&lt;/CODE&gt;: A small image just capable of allowing a device to boot.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Prefer to use core-image-base instead, because minimal is NOT supposed to be full featured image, it's only a bring up image. And add the native features you need, not only *gcc*.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Dec 2015 16:42:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hi/m-p/455219#M70949</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2015-12-01T16:42:37Z</dc:date>
    </item>
  </channel>
</rss>