<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Freezing linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454828#M70845</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me how to debug freezing system?&lt;/P&gt;&lt;P&gt;The situation is:&lt;/P&gt;&lt;P&gt;The board is powered. Uptime reaches up to 15 minutes, and then everything dies.&lt;/P&gt;&lt;P&gt;No matter if lvds display is connected (if is, then display turns black, and the console stops responding 10-15 seconds later),&lt;/P&gt;&lt;P&gt;if i.mx6 is hot or cold (i checked temperature and the same situation appears when it has 30C and 80C).&lt;/P&gt;&lt;P&gt;No message is given on console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running kernel 3.14.28 build with yocto 1.8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Sebastian Basierski&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Sep 2015 07:24:55 GMT</pubDate>
    <dc:creator>rumcajs666</dc:creator>
    <dc:date>2015-09-16T07:24:55Z</dc:date>
    <item>
      <title>Freezing linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454828#M70845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me how to debug freezing system?&lt;/P&gt;&lt;P&gt;The situation is:&lt;/P&gt;&lt;P&gt;The board is powered. Uptime reaches up to 15 minutes, and then everything dies.&lt;/P&gt;&lt;P&gt;No matter if lvds display is connected (if is, then display turns black, and the console stops responding 10-15 seconds later),&lt;/P&gt;&lt;P&gt;if i.mx6 is hot or cold (i checked temperature and the same situation appears when it has 30C and 80C).&lt;/P&gt;&lt;P&gt;No message is given on console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running kernel 3.14.28 build with yocto 1.8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Sebastian Basierski&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 07:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454828#M70845</guid>
      <dc:creator>rumcajs666</dc:creator>
      <dc:date>2015-09-16T07:24:55Z</dc:date>
    </item>
    <item>
      <title>Re: Freezing linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454829#M70846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thought also "freezing" can be caused by power management.&lt;/P&gt;&lt;P&gt;Can entering power save mods can be disabled?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 08:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454829#M70846</guid>
      <dc:creator>rumcajs666</dc:creator>
      <dc:date>2015-09-16T08:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: Freezing linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454830#M70847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;freezing can be caused by hadware or software reasons.&lt;/P&gt;&lt;P&gt;For hardware one can check:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp; power supplies, measure with oscilloscope, pay attention to ripples&lt;/P&gt;&lt;P&gt;(should be &amp;lt;5%), details can be found in Chapter 2 Design Checklist&lt;/P&gt;&lt;P&gt;i.MX6 System Development User’s Guide (rev.1, 6/2013)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-ddr errors, test memory with DDR test&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-96412"&gt;i.MX6 DDR Stress Test Tool V1.0.3&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For software one can check:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- if correct image used - for example i.MX6DQ use&amp;nbsp; :&lt;/P&gt;&lt;P&gt;L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)&lt;/P&gt;&lt;P&gt;i.MX6SX use&amp;nbsp; :&lt;/P&gt;&lt;P&gt;L3.14.28_1.0.0_iMX6SX_BUNDLE (REV L3.14.28_1.0.0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- try run minimal image and with min. frequency&lt;/P&gt;&lt;P&gt;- check that image was rebuilt with specific board ddr settings,&lt;/P&gt;&lt;P&gt;produced from DDR test&lt;/P&gt;&lt;P&gt;- check if this is caused by lcd blanking or screensaver&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/329043"&gt;Disable screen blanking on i.MX6 running Yocto&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 09:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454830#M70847</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-16T09:18:29Z</dc:date>
    </item>
    <item>
      <title>Re: Freezing linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454831#M70848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for quick answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I feel kind of stupid, because it was just screen saver;/&lt;/P&gt;&lt;P&gt;I found and fix it yesterday evening -&amp;gt; &lt;A href="http://www.armadeus.com/wiki/index.php?title=FrameBuffer" title="http://www.armadeus.com/wiki/index.php?title=FrameBuffer"&gt;Framebuffer - ArmadeusWiki&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 06:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freezing-linux/m-p/454831#M70848</guid>
      <dc:creator>rumcajs666</dc:creator>
      <dc:date>2015-09-17T06:40:45Z</dc:date>
    </item>
  </channel>
</rss>