<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issues About Set Default CPU Governor in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issues-About-Set-Default-CPU-Governor/m-p/454708#M70808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this is not possible without modifications of driver, however one can&lt;/P&gt;&lt;P&gt;limit core high operating frequency using kernel boot parameter arm_freq.&lt;/P&gt;&lt;P&gt;Please check attached Release Notes Table 6. Kernel Boot Parameters&lt;/P&gt;&lt;P&gt;p.9&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 10:22:45 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-07-29T10:22:45Z</dc:date>
    <item>
      <title>Issues About Set Default CPU Governor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-About-Set-Default-CPU-Governor/m-p/454707#M70807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How to set default CPU Governor? Not through sysfs interface manually. 3Q~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 09:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-About-Set-Default-CPU-Governor/m-p/454707#M70807</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-07-29T09:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: Issues About Set Default CPU Governor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issues-About-Set-Default-CPU-Governor/m-p/454708#M70808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this is not possible without modifications of driver, however one can&lt;/P&gt;&lt;P&gt;limit core high operating frequency using kernel boot parameter arm_freq.&lt;/P&gt;&lt;P&gt;Please check attached Release Notes Table 6. Kernel Boot Parameters&lt;/P&gt;&lt;P&gt;p.9&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 10:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issues-About-Set-Default-CPU-Governor/m-p/454708#M70808</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-29T10:22:45Z</dc:date>
    </item>
  </channel>
</rss>