<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic yocto compile in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454677#M70797</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;WARNING: The license listed MIT was not in the licenses collected for packagegroup-core-x11-xserver&lt;/P&gt;&lt;P&gt; | WARNING: The license listed MIT was not in the licenses collected for packagegroup-base&lt;/P&gt;&lt;P&gt; | WARNING: The license listed MIT was not in the licenses collected for packagegroup-fsl-gstreamer1.0&lt;/P&gt;&lt;P&gt; | WARNING: The license listed MIT was not in the licenses collected for packagegroup-base&lt;/P&gt;&lt;P&gt; | ls: cannot access /home/lja/fsl-release-bsp/build_x11/tmp/sysroots/imx6qsabresd/pkgdata/runtime-reverse/wpa-supplicant-wl18xx: No such file or directory&lt;/P&gt;&lt;P&gt; | readlink: missing operand&lt;/P&gt;&lt;P&gt; | Try `readlink --help' for more information.&lt;/P&gt;&lt;P&gt; | basename: missing operand&lt;/P&gt;&lt;P&gt; | Try `basename --help' for more information.&lt;/P&gt;&lt;P&gt; | WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt; | DEBUG: Python function do_rootfs finished&lt;/P&gt;&lt;P&gt; | ERROR: Function failed: license_create_manifest (log file is located at /home/lja/fsl-release-bsp/build_x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.3120)&lt;/P&gt;&lt;P&gt; ERROR: Task 7 (/home/lja/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt; NOTE: Tasks Summary: Attempted 6233 tasks of which 6232 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt; No currently running tasks (6232 of 6234)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; /home/lja/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs&lt;/P&gt;&lt;P&gt; Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Aug 2015 07:51:12 GMT</pubDate>
    <dc:creator>kaikaisi</dc:creator>
    <dc:date>2015-08-20T07:51:12Z</dc:date>
    <item>
      <title>yocto compile</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454677#M70797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;WARNING: The license listed MIT was not in the licenses collected for packagegroup-core-x11-xserver&lt;/P&gt;&lt;P&gt; | WARNING: The license listed MIT was not in the licenses collected for packagegroup-base&lt;/P&gt;&lt;P&gt; | WARNING: The license listed MIT was not in the licenses collected for packagegroup-fsl-gstreamer1.0&lt;/P&gt;&lt;P&gt; | WARNING: The license listed MIT was not in the licenses collected for packagegroup-base&lt;/P&gt;&lt;P&gt; | ls: cannot access /home/lja/fsl-release-bsp/build_x11/tmp/sysroots/imx6qsabresd/pkgdata/runtime-reverse/wpa-supplicant-wl18xx: No such file or directory&lt;/P&gt;&lt;P&gt; | readlink: missing operand&lt;/P&gt;&lt;P&gt; | Try `readlink --help' for more information.&lt;/P&gt;&lt;P&gt; | basename: missing operand&lt;/P&gt;&lt;P&gt; | Try `basename --help' for more information.&lt;/P&gt;&lt;P&gt; | WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt; | DEBUG: Python function do_rootfs finished&lt;/P&gt;&lt;P&gt; | ERROR: Function failed: license_create_manifest (log file is located at /home/lja/fsl-release-bsp/build_x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.3120)&lt;/P&gt;&lt;P&gt; ERROR: Task 7 (/home/lja/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt; NOTE: Tasks Summary: Attempted 6233 tasks of which 6232 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt; No currently running tasks (6232 of 6234)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; /home/lja/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs&lt;/P&gt;&lt;P&gt; Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 07:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454677#M70797</guid>
      <dc:creator>kaikaisi</dc:creator>
      <dc:date>2015-08-20T07:51:12Z</dc:date>
    </item>
    <item>
      <title>Re: yocto compile</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454678#M70798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale BSP has been released to customer thounds. And all BSP released has been QA.&lt;/P&gt;&lt;P&gt;And the build system is yocto, if have build issue with standard BSP release. Please check you build environment refer to the Yocto official site.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 09:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454678#M70798</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2015-08-21T09:44:35Z</dc:date>
    </item>
    <item>
      <title>Re: yocto compile</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454679#M70799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello kaikai si,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following up on Biyong Sun, I would recommend reviewing the documentation of the BSP that you are using, which may either be the Freescale Community BSP or the Freescale BSP Release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should have no problem baking the fsl-image-gui image as long as the environment is correctly set for your Machine(Board) and that the EULA has been accepted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2015 22:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-compile/m-p/454679#M70799</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-08-26T22:14:54Z</dc:date>
    </item>
  </channel>
</rss>