<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックXorg doesn't react on event1 with touchscreen.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454161#M70679</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the problem that xorg-server isn't refresh the cursor when I touch on the touchscreen and set the event to event1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In default xorg listens to TSLIB_TSDEVICE=/dev/input/event0 . It works but it is not accurate. So I want to do calibration but the it shows:&lt;/P&gt;&lt;P&gt;# ts_calibrate&lt;/P&gt;&lt;P&gt;xres = 800, yres = 480&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;tslib: Selected device is not a touchscreen (must support ABS and KEY event types)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my touchscreen is on event0. So I set TSLIB_TSDEVICE=/dev/input/event1 and pointercal-eventX to 1 and than I can calibrate.&lt;/P&gt;&lt;P&gt;I use a file where I write the event number and then run an init.d script to start xserver &amp;amp; matchbox:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;/usr/bin/startx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /usr/bin/matchbox-session &amp;gt; $log_file 2&amp;gt;$1 -- -pointer $inputdev vt02 &amp;amp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$inputdev is then &lt;STRONG&gt;touch-event1&lt;/STRONG&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, when I have calibrate the screen and I touch it once, the cursor moves to the touchpoint. But when I touch it again&lt;/P&gt;&lt;P&gt;nothing happens. The cursor stays where it was.&lt;/P&gt;&lt;P&gt;I checked input-device event0 in /dev and it respond me characters &amp;amp; also interrupts were counted up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I change to event0 and restart the xserver and matchbox-session and than everything works again. But not accurate.&lt;/P&gt;&lt;P&gt;Even if I change the name from pointercal-event1 (the calibration values) to pointercal-event0, it is not accurate. Like there is no calibration.&lt;/P&gt;&lt;P&gt;Also it seems that matchbox gets also stopped and started when I restart with init.d script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know where the problem is? I don't know where to look. And I haven't any ideas where the problem is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Apr 2015 12:48:05 GMT</pubDate>
    <dc:creator>andreaszeiler</dc:creator>
    <dc:date>2015-04-29T12:48:05Z</dc:date>
    <item>
      <title>Xorg doesn't react on event1 with touchscreen.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454161#M70679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the problem that xorg-server isn't refresh the cursor when I touch on the touchscreen and set the event to event1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In default xorg listens to TSLIB_TSDEVICE=/dev/input/event0 . It works but it is not accurate. So I want to do calibration but the it shows:&lt;/P&gt;&lt;P&gt;# ts_calibrate&lt;/P&gt;&lt;P&gt;xres = 800, yres = 480&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;tslib: Selected device is not a touchscreen (must support ABS and KEY event types)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my touchscreen is on event0. So I set TSLIB_TSDEVICE=/dev/input/event1 and pointercal-eventX to 1 and than I can calibrate.&lt;/P&gt;&lt;P&gt;I use a file where I write the event number and then run an init.d script to start xserver &amp;amp; matchbox:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;/usr/bin/startx&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /usr/bin/matchbox-session &amp;gt; $log_file 2&amp;gt;$1 -- -pointer $inputdev vt02 &amp;amp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$inputdev is then &lt;STRONG&gt;touch-event1&lt;/STRONG&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, when I have calibrate the screen and I touch it once, the cursor moves to the touchpoint. But when I touch it again&lt;/P&gt;&lt;P&gt;nothing happens. The cursor stays where it was.&lt;/P&gt;&lt;P&gt;I checked input-device event0 in /dev and it respond me characters &amp;amp; also interrupts were counted up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I change to event0 and restart the xserver and matchbox-session and than everything works again. But not accurate.&lt;/P&gt;&lt;P&gt;Even if I change the name from pointercal-event1 (the calibration values) to pointercal-event0, it is not accurate. Like there is no calibration.&lt;/P&gt;&lt;P&gt;Also it seems that matchbox gets also stopped and started when I restart with init.d script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know where the problem is? I don't know where to look. And I haven't any ideas where the problem is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 12:48:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454161#M70679</guid>
      <dc:creator>andreaszeiler</dc:creator>
      <dc:date>2015-04-29T12:48:05Z</dc:date>
    </item>
    <item>
      <title>Re: Xorg doesn't react on event1 with touchscreen.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454162#M70680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which BSP and device are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 17:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454162#M70680</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-05-04T17:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: Xorg doesn't react on event1 with touchscreen.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454163#M70681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we use an imx6 custom device. We use a linux kernel 3.0.35 with patches from freescale bsp 4.1.0. Also we use buildroot 2014.02.&lt;/P&gt;&lt;P&gt;When this happens, the processes for xserver (startx) and matchbox are disapeared. So I think the problem is somewhere there. I also tried tslib 1.0 but it didn't work.&lt;/P&gt;&lt;P&gt;Still I don't know which tslib I use... Buildroot downloads tslib1.1 but in the xorg there are also files for tslib... Very confusing!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 07:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xorg-doesn-t-react-on-event1-with-touchscreen/m-p/454163#M70681</guid>
      <dc:creator>andreaszeiler</dc:creator>
      <dc:date>2015-05-05T07:42:51Z</dc:date>
    </item>
  </channel>
</rss>