<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No operation LVDS touch in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-operation-LVDS-touch/m-p/454129#M70669</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;I made ​​sure that 10 inches lcd (HSD100PXN1) that work well against the Touch from i.mx6q cpu board.&lt;/P&gt;&lt;P&gt;So when you connect the 7 inches LVDS LMS700JF01-001 not touch the image is well Scary . The touch IC, MAX11801.&lt;/P&gt;&lt;P&gt;When the touch panel interrupt and I2C operation are good . However, this operation is not on the screen. The MAX11801 logo message appears that connection . Of course, X +, X-, Y +, Y- been brought up signal is properly connected.&lt;/P&gt;&lt;P&gt;Please comment why the touch no operation .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Apr 2015 10:23:48 GMT</pubDate>
    <dc:creator>kimsangyoung</dc:creator>
    <dc:date>2015-04-29T10:23:48Z</dc:date>
    <item>
      <title>No operation LVDS touch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-operation-LVDS-touch/m-p/454129#M70669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;I made ​​sure that 10 inches lcd (HSD100PXN1) that work well against the Touch from i.mx6q cpu board.&lt;/P&gt;&lt;P&gt;So when you connect the 7 inches LVDS LMS700JF01-001 not touch the image is well Scary . The touch IC, MAX11801.&lt;/P&gt;&lt;P&gt;When the touch panel interrupt and I2C operation are good . However, this operation is not on the screen. The MAX11801 logo message appears that connection . Of course, X +, X-, Y +, Y- been brought up signal is properly connected.&lt;/P&gt;&lt;P&gt;Please comment why the touch no operation .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 10:23:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-operation-LVDS-touch/m-p/454129#M70669</guid>
      <dc:creator>kimsangyoung</dc:creator>
      <dc:date>2015-04-29T10:23:48Z</dc:date>
    </item>
    <item>
      <title>Re: No operation LVDS touch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-operation-LVDS-touch/m-p/454130#M70670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for touch test one can try ts_test (tslib package in ltib)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="317078" data-objecttype="1" href="https://community.freescale.com/thread/317078"&gt;https://community.freescale.com/thread/317078&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also it makes sense on other examples:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317408"&gt;imx6 sabre-sdb and LCD touchscreen MAX11801&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/293210"&gt;Touchscreen support on IMX6 Evaluation Kit&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configuring i.MX6 boards for different screens&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/" target="_blank"&gt;http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 11:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-operation-LVDS-touch/m-p/454130#M70670</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-29T11:25:26Z</dc:date>
    </item>
  </channel>
</rss>