<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MX280 nand flash MfgTool Download error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX280-nand-flash-MfgTool-Download-error/m-p/453580#M70560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Park&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems device disconnected after attempt to load updater.sb.&lt;/P&gt;&lt;P&gt;From log updater.sb is used, while i.MX28 EVK and BSP uses updater_ivt.sb.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56908iB456C52943E96802/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL BSP by default uses *ivt images, as by default, with no OTP bits burned, &lt;/P&gt;&lt;P&gt;HAB is enabled in Open mode and requires addition of an IVT (Image Vector Table) &lt;/P&gt;&lt;P&gt;to boot stream. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 15:31:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-07-29T15:31:16Z</dc:date>
    <item>
      <title>MX280 nand flash MfgTool Download error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX280-nand-flash-MfgTool-Download-error/m-p/453579#M70559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Development Boards &lt;/P&gt;&lt;P&gt;nand flash MfgTool Download error &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We board config&lt;/P&gt;&lt;P&gt;1. MX280&lt;/P&gt;&lt;P&gt;2. NAND Flash 1Gb (K9F1G08U0D - Samsung)&lt;/P&gt;&lt;P&gt;3. DDR2 1Gb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mfgtool.log&lt;/P&gt;&lt;P&gt;Tuesday, July 28, 2015 17:50:43&lt;/P&gt;&lt;P&gt;1 - Panel A Start processing Singlechip NAND &amp;lt;LIST/&amp;gt;. Panel A Start &amp;lt;CMD/&amp;gt; type="boot" body="Recovery" file="updater.sb" timeout="10" onError="" text="Booting Update Firmware.". &lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="boot" body="Recovery" file="updater.sb" timeout="10" onError="" text="Booting Update Firmware." SUCCESS code=0x0. Panel A Start &amp;lt;CMD/&amp;gt; type="find" body="Updater" file="" timeout="180" onError="" text="". Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: Recovery OpState: WAITING_FOR_DEVICE&lt;/P&gt;&lt;P&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=0xffff0002. Panel A: Wrong device found.,failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text=""&amp;nbsp; &lt;/P&gt;&lt;P&gt;2 - Panel A Finished processing Singlechip NAND &amp;lt;LIST/&amp;gt; : FAIL code=-65534. Panel A: Reason is unknown,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should I check?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;S.W. Park&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 11:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX280-nand-flash-MfgTool-Download-error/m-p/453579#M70559</guid>
      <dc:creator>parksaewon</dc:creator>
      <dc:date>2015-07-28T11:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: MX280 nand flash MfgTool Download error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX280-nand-flash-MfgTool-Download-error/m-p/453580#M70560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Park&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems device disconnected after attempt to load updater.sb.&lt;/P&gt;&lt;P&gt;From log updater.sb is used, while i.MX28 EVK and BSP uses updater_ivt.sb.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56908iB456C52943E96802/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL BSP by default uses *ivt images, as by default, with no OTP bits burned, &lt;/P&gt;&lt;P&gt;HAB is enabled in Open mode and requires addition of an IVT (Image Vector Table) &lt;/P&gt;&lt;P&gt;to boot stream. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 15:31:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX280-nand-flash-MfgTool-Download-error/m-p/453580#M70560</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-29T15:31:16Z</dc:date>
    </item>
  </channel>
</rss>