<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Using i.MX6 UART as MIDI port</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX6-UART-as-MIDI-port/m-p/453444#M70549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seems that nobody has an experience of using i.MX6 UARTs as MIDI transceivers. Seems that you have to create your own MIDI application using existing UART driver. Note that MIDI protocol has non-standard transfer speed (31.25 kbit/s) and specific hardware interface, so, some external interface circuit is required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.midi.org/techspecs/electrispec.php" rel="nofollow"&gt;http://www.midi.org/techspecs/electrispec.php&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.midi.org/aboutmidi/glossary.php" rel="nofollow"&gt;http://www.midi.org/aboutmidi/glossary.php&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 08:41:05 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2015-09-17T08:41:05Z</dc:date>
    <item>
      <title>Using i.MX6 UART as MIDI port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX6-UART-as-MIDI-port/m-p/453443#M70548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm looking to create MIDI input/output ports on an i.MX6-based board running Linux. These ports will have to be accessible through the ALSA framework by applications running on the i.MX6.&lt;/P&gt;&lt;P&gt;Has anyone used UART interfaces on i.MX6 as MIDI ports?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 06:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX6-UART-as-MIDI-port/m-p/453443#M70548</guid>
      <dc:creator>francescolavra</dc:creator>
      <dc:date>2015-09-16T06:56:52Z</dc:date>
    </item>
    <item>
      <title>Re: Using i.MX6 UART as MIDI port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX6-UART-as-MIDI-port/m-p/453444#M70549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seems that nobody has an experience of using i.MX6 UARTs as MIDI transceivers. Seems that you have to create your own MIDI application using existing UART driver. Note that MIDI protocol has non-standard transfer speed (31.25 kbit/s) and specific hardware interface, so, some external interface circuit is required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.midi.org/techspecs/electrispec.php" rel="nofollow"&gt;http://www.midi.org/techspecs/electrispec.php&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.midi.org/aboutmidi/glossary.php" rel="nofollow"&gt;http://www.midi.org/aboutmidi/glossary.php&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 08:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-i-MX6-UART-as-MIDI-port/m-p/453444#M70549</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-09-17T08:41:05Z</dc:date>
    </item>
  </channel>
</rss>