<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: new display LVDS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/new-display-LVDS/m-p/453057#M70467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Giorgio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just as reference I'm adding a link to the other LVDS Clock thread created since these are very similar:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/353830" title="https://community.freescale.com/thread/353830"&gt;https://community.freescale.com/thread/353830&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 May 2015 20:36:45 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2015-05-01T20:36:45Z</dc:date>
    <item>
      <title>new display LVDS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/new-display-LVDS/m-p/453056#M70466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi to everybody,&lt;/P&gt;&lt;P&gt;&amp;nbsp; i coming crazy to add a new lvds to my embedded linux. I have an i.MX6 with kernel versoin 3.0.35 and FS ubuntu 12.02.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works fine, but now i have to add a new lvds with a resolution as 640 x 480. Its clock frequency is about 25.18 with a maximum of 28.33. I added in ldc.c the new resolution, but with default valued i get a clock frequency of 38 MHz. Searching on google, i found to modifify clock.c file (arch/arm/mach-mx6/clock.c) and set&lt;/P&gt;&lt;P&gt;clk_set_parent(&amp;amp;ldb_di0_clk, &amp;amp;pll5_video_main_clk);&lt;/P&gt;&lt;P&gt;Defautl value is clk_set_parent(&amp;amp;ldb_di0_clk, &amp;amp;pll2_pfd_352M);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chanching it, the clock frequency goes from 38kHz to 33, but not to 25.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thnaks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 07:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/new-display-LVDS/m-p/453056#M70466</guid>
      <dc:creator>giorgiofantin</dc:creator>
      <dc:date>2015-04-29T07:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: new display LVDS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/new-display-LVDS/m-p/453057#M70467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Giorgio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just as reference I'm adding a link to the other LVDS Clock thread created since these are very similar:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/353830" title="https://community.freescale.com/thread/353830"&gt;https://community.freescale.com/thread/353830&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 May 2015 20:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/new-display-LVDS/m-p/453057#M70467</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-05-01T20:36:45Z</dc:date>
    </item>
  </channel>
</rss>