<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB OTG on linux-imx 3.10.17 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-on-linux-imx-3-10-17/m-p/452783#M70400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working on a custom imx6 solo board based on sabre-auto board. I am using linux-imx 3.10.17 version.&lt;/P&gt;&lt;P&gt;I am getting issue with USB_OTG. Whenever the board is set in gadget mode (g_serial module is loaded), I get the connection logs. But when i remove the serial cable from the board,&lt;/P&gt;&lt;P&gt;I dont get any disconnect logs. I tried monitoring for udev events using udevadm utility. Even udevadm does not give any disconnect events.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be done to enable/ detect the disconnect events.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari Harisangam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Oct 2015 11:11:55 GMT</pubDate>
    <dc:creator>sharvariharisan</dc:creator>
    <dc:date>2015-10-12T11:11:55Z</dc:date>
    <item>
      <title>USB OTG on linux-imx 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-on-linux-imx-3-10-17/m-p/452783#M70400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working on a custom imx6 solo board based on sabre-auto board. I am using linux-imx 3.10.17 version.&lt;/P&gt;&lt;P&gt;I am getting issue with USB_OTG. Whenever the board is set in gadget mode (g_serial module is loaded), I get the connection logs. But when i remove the serial cable from the board,&lt;/P&gt;&lt;P&gt;I dont get any disconnect logs. I tried monitoring for udev events using udevadm utility. Even udevadm does not give any disconnect events.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be done to enable/ detect the disconnect events.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari Harisangam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 11:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-on-linux-imx-3-10-17/m-p/452783#M70400</guid>
      <dc:creator>sharvariharisan</dc:creator>
      <dc:date>2015-10-12T11:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG on linux-imx 3.10.17</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-on-linux-imx-3-10-17/m-p/452784#M70401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could refer to the following threads:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/364142"&gt;Re: GADGET g_serial Module&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/549457"&gt;About a USB driver of LinuxBSP for i.MX6 Solo&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 17:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-on-linux-imx-3-10-17/m-p/452784#M70401</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-10-21T17:53:59Z</dc:date>
    </item>
  </channel>
</rss>