<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6 CSI progressive BT.656 input frame rate issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452373#M70339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately there is no way to program IPU CSI so that the F bit can be ignored,&lt;/P&gt;&lt;P&gt;in general one can program it for input as generic data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Nov 2015 13:40:39 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-11-10T13:40:39Z</dc:date>
    <item>
      <title>imx6 CSI progressive BT.656 input frame rate issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452372#M70338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am using TW8836 to convert DTV progressive video into progressive BT.656 signal, and using imx6 CSI to capture it. The TW8836 BT.656 output stream cannot fix the F bit to 0 for progressive BT.656. Instead, the even and odd frames are having F=0 and F=1 respectively. Unfortunately, when I capture this progressive stream in imx6, the CSI can only recognize one particular set of SAV / EAV H/V/F code(either even frame or odd frame). As a result, I can only capture half of the frame rate comparing to my original DTV video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(For example, for a 60fps video I can only get 30fps captured stream in V4L2, no matter I set IPU_CSI_CCIR_CODE_1 to 0x40010 or 0xD0018, )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anybody please kindly teach me, how to program CSI so that the F bit can be ignored?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Tie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 10:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452372#M70338</guid>
      <dc:creator>tieliu</dc:creator>
      <dc:date>2015-11-03T10:29:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 CSI progressive BT.656 input frame rate issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452373#M70339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately there is no way to program IPU CSI so that the F bit can be ignored,&lt;/P&gt;&lt;P&gt;in general one can program it for input as generic data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 13:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452373#M70339</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-10T13:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 CSI progressive BT.656 input frame rate issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452374#M70340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;Thanks a lot for the answer. I guess I have to figure out ways fixing F-bit in the progressive stream using TW8836 register setting. (TW8836 vendor suggested fixing TW8836 register 0x067 bit5 to 1 and 0x068 bit7 to 1 but unfortunately it does not work out in my case, probably because my DTV progressive source has varying F-bit as input already).&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Tie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Nov 2015 01:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-CSI-progressive-BT-656-input-frame-rate-issue/m-p/452374#M70340</guid>
      <dc:creator>tieliu</dc:creator>
      <dc:date>2015-11-11T01:35:42Z</dc:date>
    </item>
  </channel>
</rss>