<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIssue in Wake from Standby using GPIO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452215#M70271</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are designing a system based on the iMX6DL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We want to use GPIO1_IO14 to wakeup processor from Standby mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following command is used to send processor into standby mode. "echo standby&amp;gt;/Sys/power/state"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below code is used to define the GPIO pin as wakeup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static struct gpio_keys_button imx6q_buttons[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //GPIO_BUTTON(SABRESD_VOLUME_UP, KEY_VOLUMEUP, 1, "volume-up", 0, 1),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //GPIO_BUTTON(SABRESD_VOLUME_DN, KEY_VOLUMEDOWN, 1, "volume-down", 0, 1),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //GPIO_BUTTON(SABRESD_PWR_SW_DETECT, KEY_WAKEUP, 0, "power", 1, 1),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_BUTTON(SABRESD_WAKEUP_SW, KEY_POWER, 1, "power", 1, 1),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Issue:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With above configuration sometimes processor wakes up from standby mode using GPIO1_IO14 (switch is connected to this GPIO). But most of the times processor stuck in standby mode and not able to wakeup even if we pressed wakeup switch multiple times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pankaj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2015 05:25:50 GMT</pubDate>
    <dc:creator>Pankh</dc:creator>
    <dc:date>2015-07-28T05:25:50Z</dc:date>
    <item>
      <title>Issue in Wake from Standby using GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452215#M70271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are designing a system based on the iMX6DL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We want to use GPIO1_IO14 to wakeup processor from Standby mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following command is used to send processor into standby mode. "echo standby&amp;gt;/Sys/power/state"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below code is used to define the GPIO pin as wakeup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static struct gpio_keys_button imx6q_buttons[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //GPIO_BUTTON(SABRESD_VOLUME_UP, KEY_VOLUMEUP, 1, "volume-up", 0, 1),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //GPIO_BUTTON(SABRESD_VOLUME_DN, KEY_VOLUMEDOWN, 1, "volume-down", 0, 1),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //GPIO_BUTTON(SABRESD_PWR_SW_DETECT, KEY_WAKEUP, 0, "power", 1, 1),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_BUTTON(SABRESD_WAKEUP_SW, KEY_POWER, 1, "power", 1, 1),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Issue:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With above configuration sometimes processor wakes up from standby mode using GPIO1_IO14 (switch is connected to this GPIO). But most of the times processor stuck in standby mode and not able to wakeup even if we pressed wakeup switch multiple times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pankaj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 05:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452215#M70271</guid>
      <dc:creator>Pankh</dc:creator>
      <dc:date>2015-07-28T05:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in Wake from Standby using GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452216#M70272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GPIO1_IO14 is muxed with SD2_DAT1 on Sabre SD board, so&lt;/P&gt;&lt;P&gt;one can check if SD2 is used by other application (like WiFi).&lt;/P&gt;&lt;P&gt;Also one can check wake behaviour with other GPIO, like volume-up or down.&lt;/P&gt;&lt;P&gt;Recommended to test with kernel boot parameter "ldo_active=on".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 10:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452216#M70272</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-28T10:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in Wake from Standby using GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452217#M70273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can any one let us know how to test kernel boot parameter "ldo_active=on" with&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-size: 12pt;"&gt;&lt;SPAN lang=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Linux kernel L3.0.35 version or release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Pankaj&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-size: 12pt;"&gt;&lt;SPAN lang=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2015 14:41:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452217#M70273</guid>
      <dc:creator>pankajkadu</dc:creator>
      <dc:date>2015-07-31T14:41:04Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in Wake from Standby using GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452218#M70274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at attached document p.9&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2015 16:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-in-Wake-from-Standby-using-GPIO/m-p/452218#M70274</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-08-01T16:14:41Z</dc:date>
    </item>
  </channel>
</rss>