<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: 25MHz clock from i.MX 6 GPIO16?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/25MHz-clock-from-i-MX-6-GPIO16/m-p/451511#M70085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Martin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Many customer used this solution to provide clock to PHY, GPIO_16 can output 25MHz / 50MHz / 125MHz clock. Actually, you don't need to think more about jitter, the clock can ensure PHY to work normally.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In addition, the high level of clock output from GPIO_16 is determined by NVCC_GPIO, so you should notice if it is compatible with that of PHY.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 07:30:53 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2015-07-29T07:30:53Z</dc:date>
    <item>
      <title>25MHz clock from i.MX 6 GPIO16?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/25MHz-clock-from-i-MX-6-GPIO16/m-p/451510#M70084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there are several posts about using the ENET-PLL to generate the 125MHz RGMII reference clock. But when doing this, I still need a crystal for the Ethernet PHY.&lt;/P&gt;&lt;P&gt;So I am considering using GPIO16 (mux configured for ENET_REF_CLOCK) as 25MHz clock output for the Gigabit-Ethernet PHY which itself provides the 125MHz reference clock for the RGMII.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A configuration like in &lt;A href="https://community.nxp.com/message/433249"&gt;Re: Using i.MX6 to generate 125MHz reference clock for RGMII interface&lt;/A&gt;&amp;nbsp; with the different DIV_SELECT = 00 for the PLL should do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The voltage levels of GPIO16 and the PHY's clock input are compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any pitfalls I didn't see yet?&lt;/P&gt;&lt;P&gt;What about jitter - may this be a problem? I can't find further information about the PLL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 11:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/25MHz-clock-from-i-MX-6-GPIO16/m-p/451510#M70084</guid>
      <dc:creator>mahi</dc:creator>
      <dc:date>2015-07-28T11:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: 25MHz clock from i.MX 6 GPIO16?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/25MHz-clock-from-i-MX-6-GPIO16/m-p/451511#M70085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Martin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Many customer used this solution to provide clock to PHY, GPIO_16 can output 25MHz / 50MHz / 125MHz clock. Actually, you don't need to think more about jitter, the clock can ensure PHY to work normally.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In addition, the high level of clock output from GPIO_16 is determined by NVCC_GPIO, so you should notice if it is compatible with that of PHY.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 07:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/25MHz-clock-from-i-MX-6-GPIO16/m-p/451511#M70085</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2015-07-29T07:30:53Z</dc:date>
    </item>
  </channel>
</rss>