<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MFG Tool question in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450991#M69957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; NAND-based boot loaders do not support XIP approach and should be built to run&lt;/P&gt;&lt;P&gt;in RAM area, but located in NAND (ROM). Special code (primary loader) have to pre-load&lt;/P&gt;&lt;P&gt;the bootloader to RAM area.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 04:14:48 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-09-17T04:14:48Z</dc:date>
    <item>
      <title>MFG Tool question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450990#M69956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, all&lt;/P&gt;&lt;P&gt;I'm using MFG tool for burnning bootloader.&lt;/P&gt;&lt;P&gt;When i used this, it showed to me that bootloader was built in offset 0x100000 and 0x200000.&lt;/P&gt;&lt;P&gt;But when i read the flash memory, bootloader wasn't there. Bootloader is existed in 0x100000 and A80000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why these different are occurred?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Plz, help this problem to solve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Eunseok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Sep 2015 02:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450990#M69956</guid>
      <dc:creator>eunseokjung</dc:creator>
      <dc:date>2015-09-15T02:52:49Z</dc:date>
    </item>
    <item>
      <title>Re: MFG Tool question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450991#M69957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; NAND-based boot loaders do not support XIP approach and should be built to run&lt;/P&gt;&lt;P&gt;in RAM area, but located in NAND (ROM). Special code (primary loader) have to pre-load&lt;/P&gt;&lt;P&gt;the bootloader to RAM area.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 04:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450991#M69957</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-09-17T04:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: MFG Tool question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450992#M69958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The mfg tool mechanism is "boot from usb otg".&lt;/P&gt;&lt;P&gt;It is running a entire system in the DDR including rootfs.&lt;/P&gt;&lt;P&gt;uuc is waiting for command from mfg tool by ucl2.xml.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So a customized mfg tool is a must for a customized board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 04:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Tool-question/m-p/450992#M69958</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2015-09-17T04:26:15Z</dc:date>
    </item>
  </channel>
</rss>