<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 gst_init() critical error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450537#M69858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi everyone&lt;/P&gt;&lt;P&gt;I have met a problem when &lt;/P&gt;&lt;P&gt;I using the freescale imx platform with gstreamer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified the gplay program which only call gst_init();&lt;/P&gt;&lt;P&gt;but I got the following error message.&lt;/P&gt;&lt;P&gt;==========================================&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:1309): GLib-GObject-WARNING **: cannot register existing type 'GstVorbisDec'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:1309): GLib-CRITICAL **: g_once_init_leave: assertion 'result != 0' failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:1309): GStreamer-CRITICAL **: gst_element_register: assertion 'g_type_is_a (type, GST_TYPE_ELEMENT)' failed&lt;/P&gt;&lt;P&gt;MAX resolution 1024x768&lt;/P&gt;&lt;P&gt;==========================================&lt;/P&gt;&lt;P&gt;does anyone has any idea about this problem?&lt;/P&gt;&lt;P&gt;thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Aug 2015 07:02:51 GMT</pubDate>
    <dc:creator>stevesu</dc:creator>
    <dc:date>2015-08-19T07:02:51Z</dc:date>
    <item>
      <title>gst_init() critical error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450537#M69858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi everyone&lt;/P&gt;&lt;P&gt;I have met a problem when &lt;/P&gt;&lt;P&gt;I using the freescale imx platform with gstreamer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified the gplay program which only call gst_init();&lt;/P&gt;&lt;P&gt;but I got the following error message.&lt;/P&gt;&lt;P&gt;==========================================&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:1309): GLib-GObject-WARNING **: cannot register existing type 'GstVorbisDec'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:1309): GLib-CRITICAL **: g_once_init_leave: assertion 'result != 0' failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(gst-plugin-scanner:1309): GStreamer-CRITICAL **: gst_element_register: assertion 'g_type_is_a (type, GST_TYPE_ELEMENT)' failed&lt;/P&gt;&lt;P&gt;MAX resolution 1024x768&lt;/P&gt;&lt;P&gt;==========================================&lt;/P&gt;&lt;P&gt;does anyone has any idea about this problem?&lt;/P&gt;&lt;P&gt;thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2015 07:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450537#M69858</guid>
      <dc:creator>stevesu</dc:creator>
      <dc:date>2015-08-19T07:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: gst_init() critical error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450538#M69859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you tell us, or share what changes you made to the gplay?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2015 13:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450538#M69859</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-08-19T13:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: gst_init() critical error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450539#M69860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for your reply&lt;/P&gt;&lt;P&gt;here are the codes of gplay which I modified&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void gst_api_test()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GstElement* pipeline;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GstElement* photobin;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GstElement* photo_sink;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GError&amp;nbsp; *error;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; error = NULL;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gst_init(NULL, NULL);//here i test the gst_init()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("gst_api_test S\n");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(int argc,char *argv[])&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_s8 sCommand[256];&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_s8 uri_buffer[500];&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_thread_t display_thread;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_thread_t msg_thread;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_ret_val ret_val = FSL_PLAYER_SUCCESS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_handle player_handle = NULL;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player* pplayer = NULL;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_drm_format drm_format;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_config config;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_s32 ret;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_player_s32 volume = 1;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; struct sigaction act;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; act.sa_handler = signal_handler;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sigemptyset(&amp;amp;act.sa_mask);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; act.sa_flags = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sigaction(SIGINT, &amp;amp;act, NULL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("stevesujr gplay test\n");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gst_api_test();//here i test the gst_init()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 05:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gst-init-critical-error/m-p/450539#M69860</guid>
      <dc:creator>stevesu</dc:creator>
      <dc:date>2015-09-02T05:43:40Z</dc:date>
    </item>
  </channel>
</rss>