<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ECSPI chip select and boot from SPI-Flash in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450465#M69823</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the schematics of imx6q-sabreai cpu board, NVCC_ENET,&lt;/P&gt;&lt;P&gt;NVCC_GPIO and NVCC_EIM0 have the same properties,so the power&lt;/P&gt;&lt;P&gt;behavior of U6 and V20 shoud be the same also, is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case 2(please refer the previous attachment), after I powed on the board,&lt;/P&gt;&lt;P&gt;V20 pin is always on 3.3V voltage,this shoud disable the SPI slave A,so SPI&lt;/P&gt;&lt;P&gt;slave A should have no influence to SPI-FLASH when boot up, is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61205iE16E0220A7A17DAF/image-size/large?v=v2&amp;amp;px=999" title="NVCC.PNG" alt="NVCC.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jul 2015 09:49:03 GMT</pubDate>
    <dc:creator>宗標廖</dc:creator>
    <dc:date>2015-07-03T09:49:03Z</dc:date>
    <item>
      <title>ECSPI chip select and boot from SPI-Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450463#M69821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I came to a problem when I want to boot from SPI-FLash,&lt;/P&gt;&lt;P&gt;Please refer the attachment for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;ZongbiaoLiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 01:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450463#M69821</guid>
      <dc:creator>宗標廖</dc:creator>
      <dc:date>2015-07-03T01:42:19Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI chip select and boot from SPI-Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450464#M69822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 宗標 廖 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;V20 gpio1.31 can be used by linux and mfg tools as ENET_MDC signal.&lt;/P&gt;&lt;P&gt;Also gpio1.31 has NVCC_ENET power domain, &lt;/P&gt;&lt;P&gt;while pad U6 - NVCC_GPIO, G21&amp;nbsp; -NVCC_EIM0.&lt;/P&gt;&lt;P&gt;Probably ADC has incompatible voltage levels used by these i.MX6 pads.&lt;/P&gt;&lt;P&gt;In general one can use a GPIO as chip select for SPI slave.&lt;/P&gt;&lt;P&gt;You can check if ADC is fully powered when i.MX6 begin to boot from SPI and&lt;/P&gt;&lt;P&gt;that ADC should no be powered before i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 03:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450464#M69822</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-03T03:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI chip select and boot from SPI-Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450465#M69823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the schematics of imx6q-sabreai cpu board, NVCC_ENET,&lt;/P&gt;&lt;P&gt;NVCC_GPIO and NVCC_EIM0 have the same properties,so the power&lt;/P&gt;&lt;P&gt;behavior of U6 and V20 shoud be the same also, is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case 2(please refer the previous attachment), after I powed on the board,&lt;/P&gt;&lt;P&gt;V20 pin is always on 3.3V voltage,this shoud disable the SPI slave A,so SPI&lt;/P&gt;&lt;P&gt;slave A should have no influence to SPI-FLASH when boot up, is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61205iE16E0220A7A17DAF/image-size/large?v=v2&amp;amp;px=999" title="NVCC.PNG" alt="NVCC.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 09:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450465#M69823</guid>
      <dc:creator>宗標廖</dc:creator>
      <dc:date>2015-07-03T09:49:03Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI chip select and boot from SPI-Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450466#M69824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZongbiaoLiao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you should concentrate your attention on "SPI-A" chip,&lt;/P&gt;&lt;P&gt;because it can interfere with i.MX6.&lt;/P&gt;&lt;P&gt;How it is powered ? Is it powered before i.MX6 ?&lt;/P&gt;&lt;P&gt;It should be powered after all i.MX6 power supplies become stable.&lt;/P&gt;&lt;P&gt;Regarding V20 - just for test, suggest to disconnect it from i.MX6 and &lt;/P&gt;&lt;P&gt;connect permanently to 3.3V (inactive) level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 11:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-chip-select-and-boot-from-SPI-Flash/m-p/450466#M69824</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-03T11:16:43Z</dc:date>
    </item>
  </channel>
</rss>