<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDataflash on IMX51 EVK?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177670#M6978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone ever used the dataflash (AT45DB321) on the IMX51 EVK board?&lt;/P&gt;&lt;P&gt;I have derived my own board from the EVK design but I can't get the dataflash to work as a JFFS2 filesystem. I already discovered (and corrected) a fatal flaw in mxc_dataflash.c but I'm wondering how many more problems there are.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Oct 2011 01:10:03 GMT</pubDate>
    <dc:creator>N_Coesel</dc:creator>
    <dc:date>2011-10-19T01:10:03Z</dc:date>
    <item>
      <title>Dataflash on IMX51 EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177670#M6978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone ever used the dataflash (AT45DB321) on the IMX51 EVK board?&lt;/P&gt;&lt;P&gt;I have derived my own board from the EVK design but I can't get the dataflash to work as a JFFS2 filesystem. I already discovered (and corrected) a fatal flaw in mxc_dataflash.c but I'm wondering how many more problems there are.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2011 01:10:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177670#M6978</guid>
      <dc:creator>N_Coesel</dc:creator>
      <dc:date>2011-10-19T01:10:03Z</dc:date>
    </item>
    <item>
      <title>Re: Dataflash on IMX51 EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177671#M6979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;can you r/w in u-boot?&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:eric@campro-cctv.com"&gt;eric@campro-cctv.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2011 02:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177671#M6979</guid>
      <dc:creator>DualDisplayiss1</dc:creator>
      <dc:date>2011-10-19T02:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: Dataflash on IMX51 EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177672#M6980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not using it as a boot device. It seems I can read/write using mtd_debug but when I try to mount it I get a lot of messages like:&lt;/P&gt;&lt;P&gt;Newly-erased block contained word 0x20031985 at offset 0x00277200&lt;/P&gt;&lt;P&gt;The value after word is always the same. When I dump the flash around 0x00277200 I see it is empty. I think it is some race condition between the PMIC and the flash using the same SPI interface.&lt;/P&gt;&lt;P&gt;When I try to modify a file, the JFFS2 kernel driver produces a kernel bug originating from wbuf.c.&lt;/P&gt;&lt;P&gt;I'm using kernel version 2.6.35.5.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Oct 2011 08:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dataflash-on-IMX51-EVK/m-p/177672#M6980</guid>
      <dc:creator>N_Coesel</dc:creator>
      <dc:date>2011-10-19T08:08:46Z</dc:date>
    </item>
  </channel>
</rss>