<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: exectubale has interpretor ld-linux.so.3  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450032#M69686</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have not noticed but the branch you are using is a beta version. I wonder if you can use a GA version?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Oct 2015 16:32:22 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2015-10-19T16:32:22Z</dc:date>
    <item>
      <title>exectubale has interpretor ld-linux.so.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450030#M69684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using Yocto SDK - version /opt/fsl-imx-release/1.8/ to build an exeutable and &lt;SPAN style="color: #1f497d;"&gt;the interpreter is /lib/ld-linux.so.3. I am wondering why this different from&amp;nbsp; other binaries&lt;BR /&gt;which have it as ld-linux-armhf.so.3.&amp;nbsp; My executable runs ok after creating the link ld-linux.so.3 -&amp;gt; ld-2.21.so in /lib.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Some details about the SDK used.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;The SDK itself was generate using repo branch&amp;nbsp; imx-3.14.38-6UL7D_beta . The command used is: &lt;/SPAN&gt;&lt;SPAN style="color: #1f497d;"&gt;"&lt;/SPAN&gt;&lt;SPAN style="color: #1f497d;"&gt;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.38-6UL7D_beta"&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;The machine type was imx6ulevk; The command used is &lt;/SPAN&gt;&lt;SPAN style="color: #1f497d;"&gt;MACHINE=imx6ulevk source fsl-setup-release.sh -b build_6ul -e x11; bitbake -c populate_sdk fsl-image-gui;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;SDK installed using tmp/deploy/sdk/fsl-imx-release-glibc-x86_64-fsl-image-gui-cortexa7hf-vfp-neon-toolchain-1.8.sh&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;root@imx6ulevk:~# file /bin/wl&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;/bin/wl: ELF 32-bit LSB&lt;BR /&gt;executable, ARM, EABI5 version 1 (SYSV), dynamically linked&lt;/SPAN&gt;&lt;SPAN style="color: red;"&gt;, interpreter /lib/ld-linux.so.3&lt;/SPAN&gt;&lt;SPAN style="color: #1f497d;"&gt;, for GNU/Linux 2.6.32, BuildID[sha1]=9289f54de4e622ffe2d08b9c884dc748330a4ad&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;root@imx6ulevk:~#&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;root@imx6ulevk:~# file /bin/bash &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;/bin/bash: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=044eb764ca142e79e4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~# ls -al /lib | grep ld&lt;/P&gt;&lt;P&gt;-rwxr-xr-x&amp;nbsp; 1 root root&amp;nbsp; 134392 Jul&amp;nbsp; 7 14:25 ld-2.21.so&lt;/P&gt;&lt;P&gt;lrwxrwxrwx&amp;nbsp; 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 10 Jul&amp;nbsp; 7 18:23 ld-linux-armhf.so.3 -&amp;gt; ld-2.21.so&lt;/P&gt;&lt;P&gt;lrwxrwxrwx&amp;nbsp; 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 10 Oct&amp;nbsp; 9 00:45&lt;SPAN style="color: #e23d39;"&gt; ld-linux.so.3 -&amp;gt; ld-2.21.so&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~#&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Venkat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 23:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450030#M69684</guid>
      <dc:creator>venkats</dc:creator>
      <dc:date>2015-10-09T23:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: exectubale has interpretor ld-linux.so.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450031#M69685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have checked with L3.14.28 and it seems that this has changed in L3.14.38.&lt;/P&gt;&lt;P&gt;Let me keep delving into this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Oct 2015 14:34:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450031#M69685</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-10-13T14:34:04Z</dc:date>
    </item>
    <item>
      <title>Re: exectubale has interpretor ld-linux.so.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450032#M69686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have not noticed but the branch you are using is a beta version. I wonder if you can use a GA version?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2015 16:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450032#M69686</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-10-19T16:32:22Z</dc:date>
    </item>
    <item>
      <title>Re: exectubale has interpretor ld-linux.so.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450033#M69687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the branch name for the GA version? Does that version support iMX6 Ultralite?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2015 17:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450033#M69687</guid>
      <dc:creator>venkats</dc:creator>
      <dc:date>2015-10-19T17:10:45Z</dc:date>
    </item>
    <item>
      <title>Re: exectubale has interpretor ld-linux.so.3</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450034#M69688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can find all the possible branches here:&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/refs/heads" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/refs/heads"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 20:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/exectubale-has-interpretor-ld-linux-so-3/m-p/450034#M69688</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-10-22T20:49:18Z</dc:date>
    </item>
  </channel>
</rss>