<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 Software reset trigers Serial Bootloader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448897#M69399</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check signals using logic analyzer&lt;/P&gt;&lt;P&gt;and find where boot flow stops.&lt;/P&gt;&lt;P&gt;If you are using ldo_bypass, also suggest to check &lt;/P&gt;&lt;P&gt;VDD_ARM,VDD_SOC voltages so they satisfied&lt;/P&gt;&lt;P&gt;datasheet requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2015 12:04:25 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-07-02T12:04:25Z</dc:date>
    <item>
      <title>IMX6 Software reset trigers Serial Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448894#M69396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm running a Linux 3.14.28 system on a custom iMX6DL board.&lt;/P&gt;&lt;P&gt;The system boots from an eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;My Fuses are set a follows:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;OCOTP_CFG4&amp;nbsp; &amp;lt;== 0x0000_5872&lt;BR /&gt;OCOTG_CFG5&amp;nbsp; &amp;lt;== 0x00100010&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need the ability to trigger a software reset. I do this by writing '0' to the WDOG1_WCR.SRS bit.&lt;/P&gt;&lt;P&gt;This causes the SoC to reset. But, after a ~4-5 seconds delay and the Serial Boot Loader starts (?!?!).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at 8.5.3.2, it seems that if the boot flow fails, it falls back to the USB serial downloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume the eMMC should be reset when the CPU is reset. BOOT_CFG1[1] is set -- this should assert the SD_RST signal (which is connected on our PCB). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions how to find out why resetting the CPU causes a fail with booting from eMMC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 15:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448894#M69396</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2015-07-01T15:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Software reset trigers Serial Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448895#M69397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what mode are you using ldo or ldo bypass,&lt;/P&gt;&lt;P&gt;if ldo bypass then it will not reboot, since pmic may lower&lt;/P&gt;&lt;P&gt;processor voltages below sufficient for boot limit.&lt;/P&gt;&lt;P&gt;For that reason in Sabre SD schematic wdog reboot toggle pwron&lt;/P&gt;&lt;P&gt;pmic, so both pmic and processor resets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 02:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448895#M69397</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-02T02:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Software reset trigers Serial Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448896#M69398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although I am using ldo_bypass, the CPU does reboot.&amp;nbsp;&amp;nbsp; The problem seems to be in the boot from eMMC flow. For some reason it fails, and falls-back to USB Flow.&amp;nbsp; If you look at Figures 8-10 .. 8-16, you'll see there are several places where the boot flow can fail.&amp;nbsp;&amp;nbsp; Is there any way to know where the boot flow failed? (A status register somewhere?).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other point -- I looked at the SD_RST signal, and it is asserted for 5msec when I try to reboot with the watchdog. So - eMMC is getting a RESET signal. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 07:08:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448896#M69398</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2015-07-02T07:08:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Software reset trigers Serial Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448897#M69399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check signals using logic analyzer&lt;/P&gt;&lt;P&gt;and find where boot flow stops.&lt;/P&gt;&lt;P&gt;If you are using ldo_bypass, also suggest to check &lt;/P&gt;&lt;P&gt;VDD_ARM,VDD_SOC voltages so they satisfied&lt;/P&gt;&lt;P&gt;datasheet requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 12:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448897#M69399</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-02T12:04:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Software reset trigers Serial Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448898#M69400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks -- I will try to find out what's going on. &lt;/P&gt;&lt;P&gt;Regardless, we'll add WDOG_B signal out to PMIC to ensure the entire board resets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way-- it seems worthwhile to enable the LDO mode. According to AN4725 the product life time would increase by over 50%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any reason not to enable LDO mode? (Sorry if the question is off topic).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 12:20:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448898#M69400</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2015-07-02T12:20:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Software reset trigers Serial Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448899#M69401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ldo bypass allows to reduce processor power consumption&lt;/P&gt;&lt;P&gt;due to ldo losses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 12:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Software-reset-trigers-Serial-Bootloader/m-p/448899#M69401</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-02T12:22:53Z</dc:date>
    </item>
  </channel>
</rss>