<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Android 5.0.2 GPIO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448885#M69394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kamil,&lt;/P&gt;&lt;P&gt;In this case, you could use as reference the thread below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/372070"&gt;DTS tree changes to access GPIO from linux on IMX6SL-EVK Board&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Nov 2015 00:06:34 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2015-11-10T00:06:34Z</dc:date>
    <item>
      <title>Android 5.0.2 GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448882#M69391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying set 1 input (GPIO 5.12) and one output (GPIO 1.18) on i.MX6 Solo. What exatly i should set on *.dtsi file, to get GPIO access on sys/class/gpio?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2015 10:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448882#M69391</guid>
      <dc:creator>kamilbystryk</dc:creator>
      <dc:date>2015-11-02T10:56:50Z</dc:date>
    </item>
    <item>
      <title>Re: Android 5.0.2 GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448883#M69392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kamil,&lt;/P&gt;&lt;P&gt;You could refer to the following thread, which provides tips regarding GPIO usage on Android:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/327652"&gt;How do I map Android GPIO to actual i.MX6 hardware pins&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 18:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448883#M69392</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-11-03T18:56:16Z</dc:date>
    </item>
    <item>
      <title>Re: Android 5.0.2 GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448884#M69393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlos,&lt;/P&gt;&lt;P&gt;This link shows how to use defined GPIO. I know how use GPIO when he shows in /sys/class/gpio path, however I don't have idea how configure GPIO in kernel (what in resul give access in class/gpio).&lt;/P&gt;&lt;P&gt;I found some configuration in *.dtsi file, but i don't know how configure specific lines.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2015 11:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448884#M69393</guid>
      <dc:creator>kamilbystryk</dc:creator>
      <dc:date>2015-11-04T11:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: Android 5.0.2 GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448885#M69394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kamil,&lt;/P&gt;&lt;P&gt;In this case, you could use as reference the thread below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/372070"&gt;DTS tree changes to access GPIO from linux on IMX6SL-EVK Board&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 00:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448885#M69394</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-11-10T00:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: Android 5.0.2 GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448886#M69395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlos.&lt;/P&gt;&lt;P&gt;At now, i can correctly add GPIO to filesystem, however i can't use GPIO as output (input works fine).&lt;/P&gt;&lt;P&gt;I define GPIO as:&lt;BR /&gt;MX6QDL_PAD_DISP0_DAT18__GPIO5_IO12 0x17059&lt;/P&gt;&lt;P&gt;I think, problem is in 0x17059 definition, but i don't know what is this "magic number"?&lt;/P&gt;&lt;P&gt;Second question - where i can put code to automaticly export and set GPIO at startup?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Nov 2015 11:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-5-0-2-GPIO/m-p/448886#M69395</guid>
      <dc:creator>kamilbystryk</dc:creator>
      <dc:date>2015-11-10T11:43:22Z</dc:date>
    </item>
  </channel>
</rss>