<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCorrupt display when running vivante fb tutorials</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448819#M69387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Build system: Yocto Poky ( &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://github.com/Freescale/meta-fsl-arm" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/meta-fsl-arm&lt;/A&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Linux kernel: 3.10.17_r0&lt;/P&gt;&lt;P&gt;vivante binaries: gpu-viv-bin-mx6q-3.10.17-1.0.2-hfp&lt;/P&gt;&lt;P&gt;Display: 12" (1280x800) LVDS&lt;/P&gt;&lt;P&gt;Board: Custom (based on imx solo)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vertical white lines interlaced with black and white image is been displayed on the LVDS Screen while running the sample tutorials. The snap of the LCD is attached for the reference. Terminating the tutorial gives the right resolution and the color.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frame buffer is functioning normally.&lt;/P&gt;&lt;P&gt;mode "1280x800-60" &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # D: 71.098 MHz, H: 49.374 kHz, V: 59.993 Hz &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; geometry 1280 800 1280 800 32 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; timings 14065 40 40 10 3 80 10 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; accel false &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rgba 8/16,8/8,8/0,0/0 &lt;/P&gt;&lt;P&gt;endmode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help/hint which can help us resolve this issue would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2015 06:54:59 GMT</pubDate>
    <dc:creator>kishorebhadri</dc:creator>
    <dc:date>2015-05-20T06:54:59Z</dc:date>
    <item>
      <title>Corrupt display when running vivante fb tutorials</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448819#M69387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Build system: Yocto Poky ( &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://github.com/Freescale/meta-fsl-arm" rel="nofollow" target="_blank"&gt;https://github.com/Freescale/meta-fsl-arm&lt;/A&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Linux kernel: 3.10.17_r0&lt;/P&gt;&lt;P&gt;vivante binaries: gpu-viv-bin-mx6q-3.10.17-1.0.2-hfp&lt;/P&gt;&lt;P&gt;Display: 12" (1280x800) LVDS&lt;/P&gt;&lt;P&gt;Board: Custom (based on imx solo)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vertical white lines interlaced with black and white image is been displayed on the LVDS Screen while running the sample tutorials. The snap of the LCD is attached for the reference. Terminating the tutorial gives the right resolution and the color.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frame buffer is functioning normally.&lt;/P&gt;&lt;P&gt;mode "1280x800-60" &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # D: 71.098 MHz, H: 49.374 kHz, V: 59.993 Hz &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; geometry 1280 800 1280 800 32 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; timings 14065 40 40 10 3 80 10 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; accel false &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rgba 8/16,8/8,8/0,0/0 &lt;/P&gt;&lt;P&gt;endmode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help/hint which can help us resolve this issue would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 06:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448819#M69387</guid>
      <dc:creator>kishorebhadri</dc:creator>
      <dc:date>2015-05-20T06:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupt display when running vivante fb tutorials</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448820#M69388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This problem was resolved by passing the correct boot arguments (bpp was corrected)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2015 05:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448820#M69388</guid>
      <dc:creator>kishorebhadri</dc:creator>
      <dc:date>2015-05-21T05:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: Corrupt display when running vivante fb tutorials</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448821#M69389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kishore,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please provide the bootargs that fix your issue.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 15:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Corrupt-display-when-running-vivante-fb-tutorials/m-p/448821#M69389</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-05-26T15:23:02Z</dc:date>
    </item>
  </channel>
</rss>