<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Not clear if mx53 linux DVFS enabled or not</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448683#M69346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But is there any reason why we can't use frequencies lower than 800MHz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jun 2015 09:00:40 GMT</pubDate>
    <dc:creator>bdp42</dc:creator>
    <dc:date>2015-06-15T09:00:40Z</dc:date>
    <item>
      <title>Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448677#M69340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm investigating DVFS on an IMX53 based platform running Linux. We are using the Freescale Android 10.2 BSP &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both frequency and voltage scaling appear to be enabled - as shown below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cat /sys/devices/platform/mxc_dvfs_core.0/enable&lt;/P&gt;&lt;P&gt;DVFS is enabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when I look at the min and max frequencies I see the following&lt;/P&gt;&lt;P&gt;cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_max_freq&lt;/P&gt;&lt;P&gt;800000&lt;/P&gt;&lt;P&gt;cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_min_freq&lt;/P&gt;&lt;P&gt;800000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This suggests that only one frequency is used and so no scaling is taking place.&lt;/P&gt;&lt;P&gt;Is this correct? If so how can I change this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 17:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448677#M69340</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-06-10T17:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448678#M69341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sect.20.2 Software Operation attached document&lt;/P&gt;&lt;P&gt;shows how to enable DVFS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 02:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448678#M69341</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-11T02:37:29Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448679#M69342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen this and DVFS is enabled as described in the document.&lt;/P&gt;&lt;P&gt;However the issue is that the min and max frequencies as shown by the proc file system are the same which suggests no frequency scaling can take place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The min and max values seem to derive from a table in the file kernel_imx/arch/arm/mach-mx5/mx53_wp.c. There are a number of structures ( dvfs_wp and cpu_wp ) that seem to have a bearing on this but I have not been able to find a description of their usage. I've included the relevant ones that are being used for our board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Place holder for dvfs_core setpoints for AEC parts */&lt;/P&gt;&lt;P&gt;static struct dvfs_wp dvfs_core_setpoint_aec[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {33, 0, 33, 10, 10, 0x08} }; /*800MHz*/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* working point for auto */&lt;/P&gt;&lt;P&gt;static struct cpu_wp cpu_wp_aec[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .pll_rate = 800000000,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .cpu_rate = 800000000,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .pdf = 0,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mfi = 8,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mfd = 2,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .mfn = 1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .cpu_podf = 0,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .cpu_voltage = 1100000,},&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So can frequency scaling take place if the min and max frequency are the same? Is this determined by the structures shown above and, if so, how should these structures be used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 08:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448679#M69342</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-06-11T08:10:32Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448680#M69343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;had board followed i.MX53 SMD design and has PMIC ?&lt;/P&gt;&lt;P&gt;Also could you try with linux&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABRETAB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_11.05_ER_SOURCE&lt;/A&gt;&amp;nbsp; : Linux 2.6.35 Source Code Files&lt;/P&gt;&lt;P&gt;and documentation 11.05 for i.MX53 SABRE Tablet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 09:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448680#M69343</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-11T09:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448681#M69344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have followed the mx53_ard design and we do have a PMIC (LTC3589) . Is there something different in the mx53_smd design regarding DVFS that we should be following?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2015 10:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448681#M69344</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-06-12T10:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448682#M69345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Automotive &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53AEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX53AEC&lt;/A&gt; option has only one&lt;/P&gt;&lt;P&gt;operating point (working point defined in arch/arm/mach-mx5/mx53_wp.c) 800MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22247i2BE9F152448B5BFB/image-size/large?v=v2&amp;amp;px=999" title="MX53 AEC.jpg" alt="MX53 AEC.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;opposite to consumer &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX53CEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX53CEC&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22440iCD8827377C05516F/image-size/large?v=v2&amp;amp;px=999" title="MX53 CEC.jpg" alt="MX53 CEC.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so one can consider that automotive has not DVFS mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2015 11:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448682#M69345</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-12T11:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448683#M69346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But is there any reason why we can't use frequencies lower than 800MHz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2015 09:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448683#M69346</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-06-15T09:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448684#M69347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;automotive parts were not characterized for these&lt;/P&gt;&lt;P&gt;frequencies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2015 09:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448684#M69347</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-15T09:06:30Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448685#M69348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;800Mz. is the maximum frequency of the AEC part. So it can run at lower frequencies. It just hasn't been characterised at these lower frequencies. Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2015 16:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448685#M69348</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2015-06-15T16:49:34Z</dc:date>
    </item>
    <item>
      <title>Re: Not clear if mx53 linux DVFS enabled or not</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448686#M69349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it can at lower frequencies without changing &lt;/P&gt;&lt;P&gt;core voltage. It hasn't been characterised for operation with lower&lt;/P&gt;&lt;P&gt;core voltages running at lower frequencies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 02:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Not-clear-if-mx53-linux-DVFS-enabled-or-not/m-p/448686#M69349</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-16T02:06:35Z</dc:date>
    </item>
  </channel>
</rss>