<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX6 framebuffer error with yocto</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448564#M69311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alfred,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Krisztián&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2015 08:03:07 GMT</pubDate>
    <dc:creator>krisztianbakos</dc:creator>
    <dc:date>2015-07-14T08:03:07Z</dc:date>
    <item>
      <title>iMX6 framebuffer error with yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448562#M69309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a strange error with my custom iMX6 board, running Yocto -&amp;gt; fido | meta-qt5 -&amp;gt; fido.&lt;/P&gt;&lt;P&gt;The framebuffer device comes up and I see picture on my LCD screen, but after some minutes I get the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# imx-ipuv3 2400000.ipu: ch = 9, pm_runtime_put failed:-38!&lt;/P&gt;&lt;P&gt;CPU: 0 PID: 25 Comm: kworker/0:1 Not tainted 3.14.28-1.0.0_ga+g91cf351 #7&lt;/P&gt;&lt;P&gt;Workqueue: events console_callback&lt;/P&gt;&lt;P&gt;[&amp;lt;80014644&amp;gt;] (unwind_backtrace) from [&amp;lt;8001164c&amp;gt;] (show_stack+0x10/0x14)&lt;/P&gt;&lt;P&gt;[&amp;lt;8001164c&amp;gt;] (show_stack) from [&amp;lt;8065485c&amp;gt;] (dump_stack+0x7c/0xbc)&lt;/P&gt;&lt;P&gt;[&amp;lt;8065485c&amp;gt;] (dump_stack) from [&amp;lt;80459cdc&amp;gt;] (ipu_uninit_channel+0x524/0xa7c)&lt;/P&gt;&lt;P&gt;[&amp;lt;80459cdc&amp;gt;] (ipu_uninit_channel) from [&amp;lt;802ca220&amp;gt;] (mxcfb_blank+0x80/0xb8)&lt;/P&gt;&lt;P&gt;[&amp;lt;802ca220&amp;gt;] (mxcfb_blank) from [&amp;lt;802b0550&amp;gt;] (fb_blank+0x54/0xa8)&lt;/P&gt;&lt;P&gt;[&amp;lt;802b0550&amp;gt;] (fb_blank) from [&amp;lt;802ba92c&amp;gt;] (fbcon_blank+0xf4/0x2a8)&lt;/P&gt;&lt;P&gt;[&amp;lt;802ba92c&amp;gt;] (fbcon_blank) from [&amp;lt;802f6604&amp;gt;] (do_blank_screen+0x1d4/0x284)&lt;/P&gt;&lt;P&gt;[&amp;lt;802f6604&amp;gt;] (do_blank_screen) from [&amp;lt;802f94dc&amp;gt;] (console_callback+0x88/0x15c)&lt;/P&gt;&lt;P&gt;[&amp;lt;802f94dc&amp;gt;] (console_callback) from [&amp;lt;8003ed2c&amp;gt;] (process_one_work+0xf4/0x35c)&lt;/P&gt;&lt;P&gt;[&amp;lt;8003ed2c&amp;gt;] (process_one_work) from [&amp;lt;8003f97c&amp;gt;] (worker_thread+0x130/0x3bc)&lt;/P&gt;&lt;P&gt;[&amp;lt;8003f97c&amp;gt;] (worker_thread) from [&amp;lt;80044c3c&amp;gt;] (kthread+0xcc/0xe4)&lt;/P&gt;&lt;P&gt;[&amp;lt;80044c3c&amp;gt;] (kthread) from [&amp;lt;8000e478&amp;gt;] (ret_from_fork+0x14/0x3c)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And my screen goes off (pixel clock stops)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any idea what could be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Krisztián Bakos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 12:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448562#M69309</guid>
      <dc:creator>krisztianbakos</dc:creator>
      <dc:date>2015-07-01T12:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 framebuffer error with yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448563#M69310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Krisztian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like you are getting some external exception and it is not handle correctly, you can check your dtsi files, for the default_ifmt and the pinctrl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 15:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448563#M69310</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2015-07-07T15:22:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 framebuffer error with yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448564#M69311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alfred,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Krisztián&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 08:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-framebuffer-error-with-yocto/m-p/448564#M69311</guid>
      <dc:creator>krisztianbakos</dc:creator>
      <dc:date>2015-07-14T08:03:07Z</dc:date>
    </item>
  </channel>
</rss>