<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX53 &amp;quot;Cannot start Debug&amp;quot; in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177303#M6920</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Managed to spend some time and uninstall the whole of VS2008 and the Adeneo SDK. I have started from scatch and made a note of any messages that come up. This time round I get a message concerning which debugger to execute before the next message tells me it cannot start debug. I now suspect that there is a difference between our two PC's. I have previously had CE6 installed with a Direct Insight SDK, whereas my colleagues PC has not had any CE installed. I can only think that when I installed CE6 it installed/configured an appropriate debugger.&lt;/P&gt;&lt;P&gt;I will continue to dig.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 22 Oct 2011 09:57:25 GMT</pubDate>
    <dc:creator>Wizzzbang</dc:creator>
    <dc:date>2011-10-22T09:57:25Z</dc:date>
    <item>
      <title>i.MX53 "Cannot start Debug"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177302#M6919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have two i.MX53 QSB's and I have set up my laptop and my colleagues PC up with the Compact 7 binary from Adeneo. Everything worked fine for&amp;nbsp;the first&amp;nbsp;day, then my colleague booted up the next day and tried to deploy a DEBUG build of a very simple application. VS2008 reported it was deploying and then reports "Cannot start debug." If he deploys as a RELEASE build everything works fine and the application runs.&lt;/P&gt;&lt;P&gt;He has the same installation as I do consisting of VS2008 with SP1, using the Adeneo SDK running on a Windows 7 PC. We have swapped QSB's so it is not a hardware problem.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Any Ideas?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jason.&lt;/P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Oct 2011 08:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177302#M6919</guid>
      <dc:creator>Wizzzbang</dc:creator>
      <dc:date>2011-10-14T08:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 "Cannot start Debug"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177303#M6920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Managed to spend some time and uninstall the whole of VS2008 and the Adeneo SDK. I have started from scatch and made a note of any messages that come up. This time round I get a message concerning which debugger to execute before the next message tells me it cannot start debug. I now suspect that there is a difference between our two PC's. I have previously had CE6 installed with a Direct Insight SDK, whereas my colleagues PC has not had any CE installed. I can only think that when I installed CE6 it installed/configured an appropriate debugger.&lt;/P&gt;&lt;P&gt;I will continue to dig.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Oct 2011 09:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177303#M6920</guid>
      <dc:creator>Wizzzbang</dc:creator>
      <dc:date>2011-10-22T09:57:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 "Cannot start Debug"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177304#M6921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Managed to fix the problem. Some SDK's had been installed for modile phones, which caused a problem with the executing of the debugger on the target device. Un-installed then and problem went away. :-)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2011 15:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-quot-Cannot-start-Debug-quot/m-p/177304#M6921</guid>
      <dc:creator>Wizzzbang</dc:creator>
      <dc:date>2011-10-26T15:11:16Z</dc:date>
    </item>
  </channel>
</rss>