<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Why yocto didn't generate uImage</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Why-yocto-didn-t-generate-uImage/m-p/447884#M69158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wayne Tsui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend making sure that you’re using the FSL Community BSP and not the BSP Release as the fsl-setup-release.sh is used on the FSL Release BSP, which does not support 3&lt;SUP&gt;rd&lt;/SUP&gt; party boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You didn’t mentioned which kernel you are using but starting 3.10 the kernel is created as zImage. Would you please check if that file was created?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Oct 2015 22:06:25 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2015-10-09T22:06:25Z</dc:date>
    <item>
      <title>Why yocto didn't generate uImage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-yocto-didn-t-generate-uImage/m-p/447883#M69157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use fsl-community-bsp to build image as follow:&lt;/P&gt;&lt;P&gt;$ MACHINE=imx6dl-riotboard source fsl-setup-release.sh -b riotboard-build -e fb&lt;/P&gt;&lt;P&gt;$ bitbake core-image-minimalBut I found there is no uImage at tmp/deploy/image/imx6dl-riotboard.WHY?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 02:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-yocto-didn-t-generate-uImage/m-p/447883#M69157</guid>
      <dc:creator>waynetsui</dc:creator>
      <dc:date>2015-10-09T02:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: Why yocto didn't generate uImage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-yocto-didn-t-generate-uImage/m-p/447884#M69158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wayne Tsui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend making sure that you’re using the FSL Community BSP and not the BSP Release as the fsl-setup-release.sh is used on the FSL Release BSP, which does not support 3&lt;SUP&gt;rd&lt;/SUP&gt; party boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You didn’t mentioned which kernel you are using but starting 3.10 the kernel is created as zImage. Would you please check if that file was created?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 22:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-yocto-didn-t-generate-uImage/m-p/447884#M69158</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-10-09T22:06:25Z</dc:date>
    </item>
  </channel>
</rss>