<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6q UART CTS/RTS Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447774#M69132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using a kernel 3.10.17 on a board very similar to sabre-lite board.&lt;/P&gt;&lt;P&gt;I have an HCI/ BT module connected on uart2, that needs flow control.&lt;/P&gt;&lt;P&gt;After reset, the module sends on UART TX (imx6 RX) a train of data, scanning for firmware to be downloaded from bluez hciattach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With pinmux settings for CTS and RTS commented out, i see the burst of data only on imx6 RX, as it should be, and i can upload the firmware successfully. Just after i have issues since the flow control is off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i enable pinmux ctrl pins for CTS and RTS, i see this burst of data in TX replicated on RX pin, RTS and CTS pins. And due to same train of data also in imx6 TX, i cannot upload the firmware anymore. Why this signal is now on all 4 UART pins ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Apr 2015 23:31:07 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2015-04-27T23:31:07Z</dc:date>
    <item>
      <title>imx6q UART CTS/RTS Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447774#M69132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using a kernel 3.10.17 on a board very similar to sabre-lite board.&lt;/P&gt;&lt;P&gt;I have an HCI/ BT module connected on uart2, that needs flow control.&lt;/P&gt;&lt;P&gt;After reset, the module sends on UART TX (imx6 RX) a train of data, scanning for firmware to be downloaded from bluez hciattach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With pinmux settings for CTS and RTS commented out, i see the burst of data only on imx6 RX, as it should be, and i can upload the firmware successfully. Just after i have issues since the flow control is off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i enable pinmux ctrl pins for CTS and RTS, i see this burst of data in TX replicated on RX pin, RTS and CTS pins. And due to same train of data also in imx6 TX, i cannot upload the firmware anymore. Why this signal is now on all 4 UART pins ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2015 23:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447774#M69132</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-04-27T23:31:07Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q UART CTS/RTS Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447775#M69133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; IMX6 UART has some specific implementation features. The i.MX6 DQ Reference&lt;/P&gt;&lt;P&gt;Manual provides clear description about internal signals and (external) multiplexing &lt;BR /&gt;for them. Table in the Datasheet helps to clarify it. Also - the following thread in Community &lt;BR /&gt;may be helpful.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;"i.MX6: What does the DTE/DCE in i.MX6's UART do and how are RTS and CTS affected &lt;BR /&gt; by the UARTxUFCR[DTEDCE] bit?"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="97509" data-objecttype="102" href="https://community.freescale.com/docs/DOC-97509"&gt;https://community.freescale.com/docs/DOC-97509#&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2015 03:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447775#M69133</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-28T03:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q UART CTS/RTS Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447776#M69134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are your RTS/CTS signal working then?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2015 15:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447776#M69134</guid>
      <dc:creator>marcocavallini</dc:creator>
      <dc:date>2015-04-30T15:34:35Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q UART CTS/RTS Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447777#M69135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i had some linux devicetree issues mainly, something wrong in the syntax was not enabling really the flow control on those pins. Yes, now, with proper pinmux config, it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 07:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447777#M69135</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-05-04T07:56:38Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q UART CTS/RTS Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447778#M69136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Angelo,&lt;/P&gt;&lt;P&gt;I still am struggling to make RS work.&lt;/P&gt;&lt;P&gt;Would you mind to share an excerpt of your DT please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I am doing tese settings at the moment&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="loading" href="https://community.nxp.com/thread/353966" title="https://community.freescale.com/thread/353966"&gt;https://community.freescale.com/thread/353966&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 08:35:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447778#M69136</guid>
      <dc:creator>marcocavallini</dc:creator>
      <dc:date>2015-05-05T08:35:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q UART CTS/RTS Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447779#M69137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you connected HCI BT modules directly into the iMX6 ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or Did you put any bridge between iMX6 CPU and youyr BCI BT ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Azlum&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 07:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-UART-CTS-RTS-Issue/m-p/447779#M69137</guid>
      <dc:creator>mohammedazlum</dc:creator>
      <dc:date>2015-09-23T07:06:31Z</dc:date>
    </item>
  </channel>
</rss>