<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CPU failed to boot : Error with 3.14.28 kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447633#M69116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Sharvari&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, for Solo one needs to use kernel boot parameter&lt;/P&gt;&lt;P&gt;maxcpus=1 or nosmp&lt;/P&gt;&lt;P&gt;Also recommend to look at attached Linux Guide sect.5 Enabling Solo Emulation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2015 01:15:57 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-07-28T01:15:57Z</dc:date>
    <item>
      <title>CPU failed to boot : Error with 3.14.28 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447632#M69115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am facing issue with linux-imx 3.14.28 kernel. I have a imx6solo sabre auto based board.&lt;/P&gt;&lt;P&gt;When I flash the kernel generated from Yocto (meta-fsl-arm), it gives the following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; vmalloc : 0xa0800000 - 0xff000000 (1512 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; lowmem : 0x80000000 - 0xa0000000 ( 512 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; .text : 0x80008000 - 0x806d54ac (6966 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; .init : 0x806d6000 - 0x80a6a100 (3665 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; .data : 0x80a6c000 - 0x80aaa1e0 ( 249 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp; .bss : 0x80aaa1ec - 0x80b0cc20 ( 395 kB)&lt;/P&gt;&lt;P&gt;*SLUB: HWalign=64, Order=0-3, MinObjects=0, &lt;SPAN style="color: #e23d39;"&gt;&lt;STRONG&gt;CPUs=2&lt;/STRONG&gt;&lt;/SPAN&gt;, Nodes=1*&lt;/P&gt;&lt;P&gt;Preemptible hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;&amp;nbsp; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.&lt;/P&gt;&lt;P&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2&lt;/P&gt;&lt;P&gt;NR_IRQS:16 nr_irqs:16 16&lt;/P&gt;&lt;P&gt;L310 cache controller enabled&lt;/P&gt;&lt;P&gt;l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 512 kB&lt;/P&gt;&lt;P&gt;failed to set parent of clk gpu2d_core_sel to pll2_pfd1_594m: -22&lt;/P&gt;&lt;P&gt;Switching to timer-based delay loop&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every&lt;/P&gt;&lt;P&gt;1431655765682ns&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop (skipped) preset value.. 1581.05 BogoMIPS&lt;/P&gt;&lt;P&gt;(lpj=7905280)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;/P&gt;&lt;P&gt;Setting up static identity map for 0x10516040 - 0x10516098&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;*CPU1: failed to boot: -38*&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;Brought up 1 CPUs&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #e23d39;"&gt;SMP: Total of 1 processors activated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My board is solo, but the kernel debug messages show CPUs =2.&lt;/P&gt;&lt;P&gt;Also it gives error as CPU1:failed to boot. Do i need to change any&lt;/P&gt;&lt;P&gt;configurations in Yocto or kernel config to make CPUS=1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2015 05:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447632#M69115</guid>
      <dc:creator>sharvari</dc:creator>
      <dc:date>2015-07-27T05:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: CPU failed to boot : Error with 3.14.28 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447633#M69116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Sharvari&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, for Solo one needs to use kernel boot parameter&lt;/P&gt;&lt;P&gt;maxcpus=1 or nosmp&lt;/P&gt;&lt;P&gt;Also recommend to look at attached Linux Guide sect.5 Enabling Solo Emulation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 01:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447633#M69116</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-28T01:15:57Z</dc:date>
    </item>
    <item>
      <title>Re: CPU failed to boot : Error with 3.14.28 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447634#M69117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks igor.&lt;/P&gt;&lt;P&gt;I added nosmp to kernel boot parameter and it worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Thanks&lt;/P&gt;&lt;P&gt;Sharvari Harisangam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 06:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-failed-to-boot-Error-with-3-14-28-kernel/m-p/447634#M69117</guid>
      <dc:creator>sharvari</dc:creator>
      <dc:date>2015-07-28T06:14:49Z</dc:date>
    </item>
  </channel>
</rss>