<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6Q - LDB clock's parent selection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446498#M68885</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you try &lt;/P&gt;&lt;P&gt;imx_clk_set_parent(clk[IMX6QDL_CLK_LDB_DI0_SEL],clk[IMX6QDL_CLK_PLL3_USB_OTG] );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In linuk kernel code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jun 2015 15:49:48 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2015-06-02T15:49:48Z</dc:date>
    <item>
      <title>i.MX6Q - LDB clock's parent selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446495#M68882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using imx6Q custom platform for our development which is based on sabresd platform.&lt;/P&gt;&lt;P&gt;We are using Linux 3.14.28_1.0.0-GA BSP for our development. But initially we used Linux 3.10.53_1.0.0-GA BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From Linux 3.10.53_1.0.0-GA BSP, we have referred the below Linux kernel clock file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ~/linux-imx/arch/arm/mach-imx/clk-imx6q.c&lt;/P&gt;&lt;P&gt;We understood that the below function will set the LDB clock parent and the default LDB clock parent is "pll2_pfd0_352m".&lt;/P&gt;&lt;P&gt; "init_ldb_clks"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But In Linux 3.14.28_1.0.0-GA BSP, we couldn't identify the parent clock of LDB clock.&amp;nbsp;&amp;nbsp; Please help us to understand&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our custom board, we are having LVDS0 800x480 display which is working with Linux 3.10.53_1.0.0-GA BSP.&lt;/P&gt;&lt;P&gt;The issue we are facing is,&amp;nbsp; &lt;/P&gt;&lt;P&gt;In Linux 3.14.28_1.0.0-GA BSP,&amp;nbsp; we have modified the corresponding lvds0 timing parameters in device tree. Now we are not getting the LVDS0 display.&amp;nbsp; &lt;/P&gt;&lt;P&gt;But if we keep the clock frequency as 65Mhz (as used in ~/linux-imx/arch/arm/boot/dts/imx6qdl-sabresd.dtsi) then we are able to get the display.&lt;/P&gt;&lt;P&gt;Please note that, we have changed only clock frequency value and other timing parameters are kept for 800x480 resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We believe, the LDB clock's parent is the problem for our above issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us to resolve the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ansari&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2015 16:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446495#M68882</guid>
      <dc:creator>Ansari</dc:creator>
      <dc:date>2015-05-19T16:56:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q - LDB clock's parent selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446496#M68883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know you have seens this discussion:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/355690"&gt;i.MX6Q LVDS Wrong clock issue&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if you have tried it out. I have been checking the code in 3.14.28 and it seems that it is not possible to change the parent clock the same way that in 3.10.53 (using a environment variable in u-boot).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also try the next in the clk-imx6q.c file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx_clk_set_parent(clk[IMX6QDL_CLK_LDB_DI0_SEL],clk[IMX6QDL_CLK_PLL3_USB_OTG] );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not tried that and comparing with 3.10.53 the clock is set in a totally different way, not so sure if this due a restriction. But as I see the simpler way is to modify u-boot code the way is mentioned in the above discussion. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 23:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446496#M68883</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-05-29T23:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q - LDB clock's parent selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446497#M68884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alejandro, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your input. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In U-boot level, we are not supporting any display(including LVDS) and we are supporting the displays (including LVDS) in kernel level only. &lt;/P&gt;&lt;P&gt;As per your referred community link, the LVDS clock parent settings has to be added during the "setup_display". &lt;/P&gt;&lt;P&gt;But in our case(in our custom board file) "setup_display" function is not there. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest us. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;P&gt;Ansari&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 05:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446497#M68884</guid>
      <dc:creator>Ansari</dc:creator>
      <dc:date>2015-06-02T05:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q - LDB clock's parent selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446498#M68885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you try &lt;/P&gt;&lt;P&gt;imx_clk_set_parent(clk[IMX6QDL_CLK_LDB_DI0_SEL],clk[IMX6QDL_CLK_PLL3_USB_OTG] );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In linuk kernel code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 15:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-LDB-clock-s-parent-selection/m-p/446498#M68885</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-06-02T15:49:48Z</dc:date>
    </item>
  </channel>
</rss>