<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Absolute Maximum Ratings for VINSW2 of PF0100 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Absolute-Maximum-Ratings-for-VINSW2-of-PF0100/m-p/446391#M68857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuuki&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;based on Table 4,5&amp;nbsp; Absolute Maximum Ratings&lt;/P&gt;&lt;P&gt;are -0.3 to 4.8V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Nov 2015 01:37:32 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-11-27T01:37:32Z</dc:date>
    <item>
      <title>Absolute Maximum Ratings for VINSW2 of PF0100</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Absolute-Maximum-Ratings-for-VINSW2-of-PF0100/m-p/446390#M68856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I check VIN of SW2 of PF0100.&lt;/P&gt;&lt;P&gt;I checked Absolute Maximum Ratings of the PF0100 data sheet.&lt;BR /&gt;- Table 5. Absolute Maximum Ratings(P.11)&lt;/P&gt;&lt;P&gt;Furthermore, I checked the following point.&lt;BR /&gt;- SW2 Specifications(P.63)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I was not able to find a description of VINSW2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found Max Rating in Pin Definitions.&lt;BR /&gt;- Table 4. PF0100 Pin Definitions(P.9)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should I refer to this Tabel 4 as Absolute Maximum Ratings for VINSW2?&lt;BR /&gt;(In this case I do not understand the minimum value.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 06:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Absolute-Maximum-Ratings-for-VINSW2-of-PF0100/m-p/446390#M68856</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2015-11-26T06:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: Absolute Maximum Ratings for VINSW2 of PF0100</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Absolute-Maximum-Ratings-for-VINSW2-of-PF0100/m-p/446391#M68857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuuki&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;based on Table 4,5&amp;nbsp; Absolute Maximum Ratings&lt;/P&gt;&lt;P&gt;are -0.3 to 4.8V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 01:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Absolute-Maximum-Ratings-for-VINSW2-of-PF0100/m-p/446391#M68857</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-27T01:37:32Z</dc:date>
    </item>
  </channel>
</rss>