<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX53 TZIC PRIORITY_MASK register setting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-TZIC-PRIORITY-MASK-register-setting/m-p/446236#M68818</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm confusing about PRIORITY_MASK setting in TZIC of i.MX53.&lt;BR /&gt;I beleive &lt;STRONG&gt;highest priority is 0&lt;/STRONG&gt; but usage describe as following.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The ARM platform will&lt;/P&gt;&lt;P&gt;only receive an interrupt if there is a pending interrupt with a priority &lt;STRONG&gt;higher&lt;/STRONG&gt; than the&lt;/P&gt;&lt;P&gt;value in this register. If an interrupt source asserts and its priority is &lt;STRONG&gt;equal to or lower&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;than the priority mask value, it will not cause an interrupt to the ARM platform.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does "higher" mean (PRIORITYn &amp;lt; PRIORITY_MASK)?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Does "equal to or lower" mean (PRIORITYn &amp;gt;= PRIORITY_MASK)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone clarify for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2015 05:11:53 GMT</pubDate>
    <dc:creator>torus1000</dc:creator>
    <dc:date>2015-08-18T05:11:53Z</dc:date>
    <item>
      <title>i.MX53 TZIC PRIORITY_MASK register setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-TZIC-PRIORITY-MASK-register-setting/m-p/446236#M68818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm confusing about PRIORITY_MASK setting in TZIC of i.MX53.&lt;BR /&gt;I beleive &lt;STRONG&gt;highest priority is 0&lt;/STRONG&gt; but usage describe as following.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;The ARM platform will&lt;/P&gt;&lt;P&gt;only receive an interrupt if there is a pending interrupt with a priority &lt;STRONG&gt;higher&lt;/STRONG&gt; than the&lt;/P&gt;&lt;P&gt;value in this register. If an interrupt source asserts and its priority is &lt;STRONG&gt;equal to or lower&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;than the priority mask value, it will not cause an interrupt to the ARM platform.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does "higher" mean (PRIORITYn &amp;lt; PRIORITY_MASK)?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Does "equal to or lower" mean (PRIORITYn &amp;gt;= PRIORITY_MASK)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone clarify for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2015 05:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-TZIC-PRIORITY-MASK-register-setting/m-p/446236#M68818</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2015-08-18T05:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 TZIC PRIORITY_MASK register setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-TZIC-PRIORITY-MASK-register-setting/m-p/446237#M68819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torus1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are right, highest priority value is 0, as describes&lt;/P&gt;&lt;P&gt;below part of RM&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54097iA046944AFEF1B6FF/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2015 06:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-TZIC-PRIORITY-MASK-register-setting/m-p/446237#M68819</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-08-18T06:10:33Z</dc:date>
    </item>
  </channel>
</rss>