<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Stressapptest crashes immediately</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446222#M68815</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All -&lt;/P&gt;&lt;P&gt;The effect of reducing the resistor value of the ZQ resistor is to increase the drive strength of all your signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;240 Ohms is specified by the JEDEC standards as the corect resistor value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will admit that, for testing purposes only, I have reduced the ZQ resistor value a few times, usually on the DDR device side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the correct way to increase drive strength is to do this in the configuartion registers. If you have IOMUX registers set to DSE of '101' or '110', try increasing them up to maximum value: '111'. If that works, then you can selectively reduce drive strength until you achieve a setting you like. For the DDR devices, this is done in the mode registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP does not recommend using different ZQ resistor values than those stated in the device datasheet. For i.MX6 processors, this value is 240 Ohm 1% resistors. If a customer uses a different value, the customer assumes all risk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A note about the DDR Stress test: We have been finding publically available stress tests that seem to push harder, and in different configurations than the DDR Stress test.&amp;nbsp; The stress test that NXP uses is provided "as is". We do work to evolving our stress test to be even more stressful for our internal use, but if you find something even more stressful in a particular operating system, by all means, use every tool available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Mar 2016 16:14:17 GMT</pubDate>
    <dc:creator>TheAdmiral</dc:creator>
    <dc:date>2016-03-03T16:14:17Z</dc:date>
    <item>
      <title>Stressapptest crashes immediately</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446218#M68811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello out there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm facing a DDR3 problem on a custom design with i.MX6. I calibrated the DDR3 with DDR Stress Test (2.2.0).&lt;/P&gt;&lt;P&gt;Did the write leveling succesfully, the dqs gating succesfully as well as the read and write calibration.&lt;/P&gt;&lt;P&gt;The DDR stress tester runs without any errors. (Here are the calibration results)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; MMDC registers updated from calibration &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write leveling calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00150019&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x0017000E&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x00040019&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x0012001B&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Read DQS Gating calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL0 PHY0 (0x021b083c) = 0x43200324&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL1 PHY0 (0x021b0840) = 0x026C0268&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL0 PHY1 (0x021b483c) = 0x43080314&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL1 PHY1 (0x021b4840) = 0x03140268&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Read calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPRDDLCTL PHY0 (0x021b0848) = 0x40383438&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPRDDLCTL PHY1 (0x021b4848) = 0x3C383442&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPWRDLCTL PHY0 (0x021b0850) = 0x342E3A34&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPWRDLCTL PHY1 (0x021b4850) = 0x402E423A&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Success: DDR calibration completed!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As soon as I boot into linux and run the stressapptest from google it crashes almost immediately.&lt;/P&gt;&lt;P&gt;Sometimes I get some miscompare results showing that the two least significant bytes are wrong.&lt;/P&gt;&lt;P&gt;But most of the time the application just crashes with different types of errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51801i0B76BC25B9B7A0C6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_13.png" alt="pastedImage_13.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone any idea what is happening here ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanx for your help &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Norbert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2015 11:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446218#M68811</guid>
      <dc:creator>stefanovski</dc:creator>
      <dc:date>2015-11-02T11:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: Stressapptest crashes immediately</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446219#M68812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. &lt;BR /&gt;&amp;nbsp;&amp;nbsp; Please try to run FSL DDR Stress tool during long time (at least several hours).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. &lt;/P&gt;&lt;P&gt;&amp;nbsp; Have You used the same DDR initalization setting as for DDR stress (after calibration) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2015 07:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446219#M68812</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-11-06T07:06:53Z</dc:date>
    </item>
    <item>
      <title>Re: Stressapptest crashes immediately</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446220#M68813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes i ran the &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; FSL DDR Stress tool for several hours and i used the settings i got from calibration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Believe it or not, i fixed the problem by adjusting the ZQ resistor at the i.MX6 a little bit downwards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;because i had the feeling that the impedances on my board do not match the 50 Ohm, 100 Ohm&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;good enough. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Now stressapptest is running without errors. I still can't understand how &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;FSL DDR Stress tool and &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;memtester could'nt make out any errors while &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;stressapptest crashed immediately. Mysterious.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2015 05:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446220#M68813</guid>
      <dc:creator>stefanovski</dc:creator>
      <dc:date>2015-11-13T05:30:57Z</dc:date>
    </item>
    <item>
      <title>Re: Stressapptest crashes immediately</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446221#M68814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;:smileyconfused:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2015 06:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446221#M68814</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-11-13T06:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: Stressapptest crashes immediately</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446222#M68815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All -&lt;/P&gt;&lt;P&gt;The effect of reducing the resistor value of the ZQ resistor is to increase the drive strength of all your signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;240 Ohms is specified by the JEDEC standards as the corect resistor value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will admit that, for testing purposes only, I have reduced the ZQ resistor value a few times, usually on the DDR device side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the correct way to increase drive strength is to do this in the configuartion registers. If you have IOMUX registers set to DSE of '101' or '110', try increasing them up to maximum value: '111'. If that works, then you can selectively reduce drive strength until you achieve a setting you like. For the DDR devices, this is done in the mode registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP does not recommend using different ZQ resistor values than those stated in the device datasheet. For i.MX6 processors, this value is 240 Ohm 1% resistors. If a customer uses a different value, the customer assumes all risk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A note about the DDR Stress test: We have been finding publically available stress tests that seem to push harder, and in different configurations than the DDR Stress test.&amp;nbsp; The stress test that NXP uses is provided "as is". We do work to evolving our stress test to be even more stressful for our internal use, but if you find something even more stressful in a particular operating system, by all means, use every tool available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 16:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stressapptest-crashes-immediately/m-p/446222#M68815</guid>
      <dc:creator>TheAdmiral</dc:creator>
      <dc:date>2016-03-03T16:14:17Z</dc:date>
    </item>
  </channel>
</rss>