<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKITPFGUI issues with Interrupts</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/KITPFGUI-issues-with-Interrupts/m-p/445604#M68695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am currently testing our current configuration with the PF0100 connected to the KITPFGUI tool and we have several questions :&lt;/P&gt;&lt;P&gt;1.Can we monitor in real-time the current consumption of each Buck and LDOs and the global consumption of the PF0100 ?&lt;/P&gt;&lt;P&gt;2.How the Interrupts are brought up to the KITPFGUI as the INTB pin is not connected to the programmer ? Through the I2C bus ?&lt;/P&gt;&lt;P&gt;We need to check if we have no over-current alarms on each DC-DC.&lt;/P&gt;&lt;P&gt;My best regards,&lt;/P&gt;&lt;P&gt;Xavier.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Oct 2015 11:07:56 GMT</pubDate>
    <dc:creator>xaviercarcelle</dc:creator>
    <dc:date>2015-10-30T11:07:56Z</dc:date>
    <item>
      <title>KITPFGUI issues with Interrupts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/KITPFGUI-issues-with-Interrupts/m-p/445604#M68695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am currently testing our current configuration with the PF0100 connected to the KITPFGUI tool and we have several questions :&lt;/P&gt;&lt;P&gt;1.Can we monitor in real-time the current consumption of each Buck and LDOs and the global consumption of the PF0100 ?&lt;/P&gt;&lt;P&gt;2.How the Interrupts are brought up to the KITPFGUI as the INTB pin is not connected to the programmer ? Through the I2C bus ?&lt;/P&gt;&lt;P&gt;We need to check if we have no over-current alarms on each DC-DC.&lt;/P&gt;&lt;P&gt;My best regards,&lt;/P&gt;&lt;P&gt;Xavier.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 11:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/KITPFGUI-issues-with-Interrupts/m-p/445604#M68695</guid>
      <dc:creator>xaviercarcelle</dc:creator>
      <dc:date>2015-10-30T11:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: KITPFGUI issues with Interrupts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/KITPFGUI-issues-with-Interrupts/m-p/445605#M68696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xavier,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[A1] It is not possible to measure the real time current on the DC-DC regulators using the KITPFGUI, it just send an alert when there is an over-current event.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[A2] You can check the source of the interrupts by checking the INTSTATx Registers of the MMPF0100 to check if there is an over-current on each DC-DC regulator.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2015 13:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/KITPFGUI-issues-with-Interrupts/m-p/445605#M68696</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-11-04T13:21:24Z</dc:date>
    </item>
  </channel>
</rss>