<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックConnect 2 SABRE LITE boards over ethernet</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445302#M68622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P dir="ltr"&gt;I am trying to connect 2 sabre lite iMx6 Quad boards (from boundary devices) over Ethernet.&lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;Both boards run Android Lollipop.&lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;If I connect them via an Ethernet Switch, the lights on the Ethernet connectors light up and blink. I can also ping from one board to the other. I also can open a TCP/IP socket and send data back and forth.&lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;When I connect the 2 boards directly to each other using a cross over ethernet cable, the lights do not blink and I cannot ping from one board to another. &lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;Has anybody tried this before?&lt;/P&gt;&lt;P dir="ltr"&gt;Do you have any suggestions to solve this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Oct 2015 18:28:47 GMT</pubDate>
    <dc:creator>davidmuscat</dc:creator>
    <dc:date>2015-10-09T18:28:47Z</dc:date>
    <item>
      <title>Connect 2 SABRE LITE boards over ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445302#M68622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P dir="ltr"&gt;I am trying to connect 2 sabre lite iMx6 Quad boards (from boundary devices) over Ethernet.&lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;Both boards run Android Lollipop.&lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;If I connect them via an Ethernet Switch, the lights on the Ethernet connectors light up and blink. I can also ping from one board to the other. I also can open a TCP/IP socket and send data back and forth.&lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;When I connect the 2 boards directly to each other using a cross over ethernet cable, the lights do not blink and I cannot ping from one board to another. &lt;/P&gt;&lt;P dir="ltr"&gt;&lt;/P&gt;&lt;P dir="ltr"&gt;Has anybody tried this before?&lt;/P&gt;&lt;P dir="ltr"&gt;Do you have any suggestions to solve this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 18:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445302#M68622</guid>
      <dc:creator>davidmuscat</dc:creator>
      <dc:date>2015-10-09T18:28:47Z</dc:date>
    </item>
    <item>
      <title>Re: Connect 2 SABRE LITE boards over ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445303#M68623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you configured IP addresses of each board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 07:09:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445303#M68623</guid>
      <dc:creator>mike_susen</dc:creator>
      <dc:date>2015-10-14T07:09:24Z</dc:date>
    </item>
    <item>
      <title>Re: Connect 2 SABRE LITE boards over ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445304#M68624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure that IP is configured respectively.&lt;/P&gt;&lt;P&gt;I mean both boards have static IP addresses in the same network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 07:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445304#M68624</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-10-14T07:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: Connect 2 SABRE LITE boards over ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445305#M68625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I have configured both boards to have static IP addresses (192.168.1.2 and 192.168.1.3)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 16:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445305#M68625</guid>
      <dc:creator>davidmuscat</dc:creator>
      <dc:date>2015-10-14T16:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: Connect 2 SABRE LITE boards over ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445306#M68626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also please make sure that you are using right cable.&lt;/P&gt;&lt;P&gt;I mean you need to use crossover cable when you are connecting the devices directly (without a switch).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Nov 2015 05:28:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-2-SABRE-LITE-boards-over-ethernet/m-p/445306#M68626</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-11-05T05:28:10Z</dc:date>
    </item>
  </channel>
</rss>