<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LRADC sampling rate in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445086#M68599</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have written a driver for capturing data from LRADC 6 channel. I am giving a test input using a signal generator and seeing if the data is captured properly.&lt;/P&gt;&lt;P&gt;Everything is working fine but the best sampling rate i am able to acheive is aroung 100 Khz(capturing 6000 samples in 60 ms). I have set the CYCLE_TIME in HW_LRADC_CTRL3 to 6 Mhz but still the sampling rate. Is it the best i can acheive using LRADC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board used is IMX 28 and linux kernel is 2.6.31&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Nov 2015 04:16:49 GMT</pubDate>
    <dc:creator>imravi</dc:creator>
    <dc:date>2015-11-27T04:16:49Z</dc:date>
    <item>
      <title>LRADC sampling rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445086#M68599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have written a driver for capturing data from LRADC 6 channel. I am giving a test input using a signal generator and seeing if the data is captured properly.&lt;/P&gt;&lt;P&gt;Everything is working fine but the best sampling rate i am able to acheive is aroung 100 Khz(capturing 6000 samples in 60 ms). I have set the CYCLE_TIME in HW_LRADC_CTRL3 to 6 Mhz but still the sampling rate. Is it the best i can acheive using LRADC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board used is IMX 28 and linux kernel is 2.6.31&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 04:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445086#M68599</guid>
      <dc:creator>imravi</dc:creator>
      <dc:date>2015-11-27T04:16:49Z</dc:date>
    </item>
    <item>
      <title>Re: LRADC sampling rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445087#M68600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ravi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;low sample rate may be caused by delays from operating system,&lt;/P&gt;&lt;P&gt;one can try with os-less (bare metal) test, using i.MX28 OBDS (touch_screen.c)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lab and Test Software (1)&lt;/P&gt;&lt;P&gt;On-Board Diagnostic Suit for the i.MX28 (REV 1)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx28-processors/i.mx28-evaluation-kit:MCIMX28EVKJ?fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow"&gt;http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx28-processors/i.mx28-evaluation-kit:MCIMX28EVKJ?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 07:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445087#M68600</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-27T07:12:24Z</dc:date>
    </item>
    <item>
      <title>Re: LRADC sampling rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445088#M68601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the Reference manual of IMX28 with 6Mhz set in the &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;HW_LRADC_CTRL3 register , the sampling speed should be (6*10^6)/13 which comes to 461.5 Khz sampling rate. But the effective rate of sampling is 100 Khz. Can this much of delay be caused by the OS layer. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 09:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445088#M68601</guid>
      <dc:creator>imravi</dc:creator>
      <dc:date>2015-11-27T09:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: LRADC sampling rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445089#M68602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, in general such delays may be caused by OS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 10:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LRADC-sampling-rate/m-p/445089#M68602</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-27T10:09:05Z</dc:date>
    </item>
  </channel>
</rss>