<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Mainline Kernel V4 for iMX28</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445031#M68588</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jörg,&lt;/P&gt;&lt;P&gt;our problems result from using an old/wrong bootloader as we made there some changes due to our requirements. So to all who want porting to a newer 3.x/4.x kernel the advice take the appropriate bootloader.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jul 2015 08:14:57 GMT</pubDate>
    <dc:creator>michaelkoelbl</dc:creator>
    <dc:date>2015-07-08T08:14:57Z</dc:date>
    <item>
      <title>Mainline Kernel V4 for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445026#M68583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We want to change from Freescale's 2.6 kernel to Mainline kernel. As now V4.x is available my question: Has anyone successfully got a V4 kernel running? Is there an instruction available? Or should we use V3.x instead?&lt;/P&gt;&lt;P&gt;We have a custom board based on the EVK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 06:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445026#M68583</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2015-07-01T06:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: Mainline Kernel V4 for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445027#M68584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Without any difficulties we have a custom i.MX28 board running with Linux Kernel 4.0.x. The Freescalers are very active in developing the mainline Kernel :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 05:01:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445027#M68584</guid>
      <dc:creator>jörg_krause</dc:creator>
      <dc:date>2015-07-03T05:01:56Z</dc:date>
    </item>
    <item>
      <title>Re: Mainline Kernel V4 for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445028#M68585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jörg,&lt;/P&gt;&lt;P&gt;can you tell me which bootloader (and which version) you're using?&lt;/P&gt;&lt;P&gt;Thanks from Bavaria&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2015 16:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445028#M68585</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2015-07-06T16:06:53Z</dc:date>
    </item>
    <item>
      <title>Re: Mainline Kernel V4 for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445029#M68586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the current mainline kernel support most of the features in Freescale 2.6.35 downstream kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest to use the Linux 4.1 because it will get longterm support in the near future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you want to migrate from the old downstream kernel, you will need to build a new BSP for the custom board based on &lt;A href="http://events.linuxfoundation.org/sites/events/files/slides/petazzoni-device-tree-dummies.pdf"&gt;Device Tree&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Since your design bases on EVK you could copy arch/arm/boot/dts/imx28-evk.dts and modify it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2015 17:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445029#M68586</guid>
      <dc:creator>lategoodbye</dc:creator>
      <dc:date>2015-07-06T17:32:35Z</dc:date>
    </item>
    <item>
      <title>Re: Mainline Kernel V4 for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445030#M68587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're using U-Boot version 2015.01 - but 2015.04 is also appropriate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2015 19:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445030#M68587</guid>
      <dc:creator>jörg_krause</dc:creator>
      <dc:date>2015-07-06T19:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: Mainline Kernel V4 for iMX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445031#M68588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jörg,&lt;/P&gt;&lt;P&gt;our problems result from using an old/wrong bootloader as we made there some changes due to our requirements. So to all who want porting to a newer 3.x/4.x kernel the advice take the appropriate bootloader.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 08:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mainline-Kernel-V4-for-iMX28/m-p/445031#M68588</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2015-07-08T08:14:57Z</dc:date>
    </item>
  </channel>
</rss>