<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: (i.MX280) Firmware update by Mfgtools fails in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444478#M68438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the suggestion.&lt;/P&gt;&lt;P&gt;The board has only two boot options, nand and usb.&lt;/P&gt;&lt;P&gt;As we cannot update the firmware, there is no way to run memory test...&lt;/P&gt;&lt;P&gt;I suppose we'd better forget about the board and try another one to test new ddr2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the power of the board and there was no problem with it.&lt;/P&gt;&lt;P&gt;(The output voltage of VDD4P2 was low as the startup process is not completed.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hikaru&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Oct 2015 08:11:24 GMT</pubDate>
    <dc:creator>hikaruuruno</dc:creator>
    <dc:date>2015-10-09T08:11:24Z</dc:date>
    <item>
      <title>(i.MX280) Firmware update by Mfgtools fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444476#M68436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are having a trouble with updating firmware by Mfgtools.&lt;BR /&gt;When we try to update firmware for a certain custom board by Mfgtools, it fails with the following log;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Friday, October 02, 2015 11:37:28&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;1 - Panel A Start processing Singlechip NAND uboot1 kernel2 UBI &amp;lt;LIST/&amp;gt;.&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Panel A Start &amp;lt;CMD/&amp;gt; type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware.".&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" onError="" text="Booting Update Firmware." SUCCESS code=0x0.&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Panel A Start &amp;lt;CMD/&amp;gt; type="find" body="Updater" file="" timeout="180" onError="" text="".&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: Recovery OpState: WAITING_FOR_DEVICE&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=0xffff0002.&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Panel A: Wrong device found.,failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text=""&amp;nbsp; &lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;2 - Panel A Finished processing Singlechip NAND uboot1 kernel2 UBI &amp;lt;LIST/&amp;gt; : FAIL code=-65534.&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Panel A: Reason is unknown,&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The serial log is as follows;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;PowerPrep start initialize power...&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Configured for 5v only power source.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Battery powered operation disabled.&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;LLLCMay 26 201509:08:44&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;FRAC 0x92925552&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;memory type is DDR2&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wait for ddr ready 1power 0x00820710&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Frac 0x92925552&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;start change cpu freq&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;hbus 0x00000003&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;cpu 0x00010001&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;LLLLLLLFLCLFLLJ&lt;/EM&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #3a0699;"&gt;&lt;EM&gt;Undefined Ins&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know what's wrong with the board?&lt;BR /&gt;The chip is i.MX280.&lt;/P&gt;&lt;P&gt;The configuration of the board is 5v-only, and it has a nand flash (boot device) and a ddr2 ram.&lt;BR /&gt;I searched the Community but could not find the solution for this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It just happens to a certain board.&lt;BR /&gt;There was no problem with the board until we replace the ddr2 chip on the board.&lt;BR /&gt;The firmware (Linux) written on the board before replacing the ddr2 could be booted without problem after replacing the ddr2.&lt;BR /&gt;Thus I assumed that replacing ddr2 was successful. (If ddr2 is not working, boot cannot be finished.)&lt;BR /&gt;Usually, updating firmware takes about 60 seconds. But when I tried it for the first time after replacing ddr2, it didn't finished for ca. 120 seconds. (Unfortunately, I wasn't taking log then...)&lt;BR /&gt;So I severed the power and tried again.&lt;BR /&gt;From then on, the log's been as I described above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume either NAND or the new DDR2 is causing the problem.&lt;BR /&gt;But since there is not many boards to spare, we'd like to identify the cause of the problem before replacing ICs with spare ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Hikaru Uruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Oct 2015 08:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444476#M68436</guid>
      <dc:creator>hikaruuruno</dc:creator>
      <dc:date>2015-10-08T08:25:11Z</dc:date>
    </item>
    <item>
      <title>Re: (i.MX280) Firmware update by Mfgtools fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444477#M68437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hikaru&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Undefined Ins" and reboot may lead to suggestion that&lt;/P&gt;&lt;P&gt;ddr memory is not working properly, suggest to run ddr test.&lt;/P&gt;&lt;P&gt;Also it may be suggested to check power lines on that board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 01:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444477#M68437</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-09T01:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: (i.MX280) Firmware update by Mfgtools fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444478#M68438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the suggestion.&lt;/P&gt;&lt;P&gt;The board has only two boot options, nand and usb.&lt;/P&gt;&lt;P&gt;As we cannot update the firmware, there is no way to run memory test...&lt;/P&gt;&lt;P&gt;I suppose we'd better forget about the board and try another one to test new ddr2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the power of the board and there was no problem with it.&lt;/P&gt;&lt;P&gt;(The output voltage of VDD4P2 was low as the startup process is not completed.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hikaru&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 08:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444478#M68438</guid>
      <dc:creator>hikaruuruno</dc:creator>
      <dc:date>2015-10-09T08:11:24Z</dc:date>
    </item>
    <item>
      <title>Re: (i.MX280) Firmware update by Mfgtools fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444479#M68439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hikaru&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are right, one can try to replace (or&lt;/P&gt;&lt;P&gt;resolder) ddr part&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 11:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX280-Firmware-update-by-Mfgtools-fails/m-p/444479#M68439</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-09T11:08:19Z</dc:date>
    </item>
  </channel>
</rss>