<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SNVS_LPCR [DEBOUNCE] bits</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-LPCR-DEBOUNCE-bits/m-p/444063#M68344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to modify the DEBOUNCE bits in the SNVS_LPCR register however it doesn't seem to be working. I have searched this community and have noticed some descrepencies in the documentation. This post seems to indicate this bit field is present:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/475422"&gt;Re: imx6 Off to On transition time?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While this one seems to indicate the opposite:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95582"&gt;Q&amp;amp;amp;A: ON_TIME and DEBOUNCE bit fields of SNVS_LPCR register readable?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please confirm if this bit is indeed modifiable and if so, how to do it? thanks. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Sep 2015 15:21:03 GMT</pubDate>
    <dc:creator>julesg</dc:creator>
    <dc:date>2015-09-11T15:21:03Z</dc:date>
    <item>
      <title>SNVS_LPCR [DEBOUNCE] bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-LPCR-DEBOUNCE-bits/m-p/444063#M68344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to modify the DEBOUNCE bits in the SNVS_LPCR register however it doesn't seem to be working. I have searched this community and have noticed some descrepencies in the documentation. This post seems to indicate this bit field is present:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/475422"&gt;Re: imx6 Off to On transition time?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While this one seems to indicate the opposite:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95582"&gt;Q&amp;amp;amp;A: ON_TIME and DEBOUNCE bit fields of SNVS_LPCR register readable?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please confirm if this bit is indeed modifiable and if so, how to do it? thanks. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 15:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SNVS-LPCR-DEBOUNCE-bits/m-p/444063#M68344</guid>
      <dc:creator>julesg</dc:creator>
      <dc:date>2015-09-11T15:21:03Z</dc:date>
    </item>
    <item>
      <title>Re: SNVS_LPCR [DEBOUNCE] bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SNVS-LPCR-DEBOUNCE-bits/m-p/444064#M68345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Jules&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DEBOUNCE bits are not writable, this is doc issue as noted in second post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Sep 2015 12:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SNVS-LPCR-DEBOUNCE-bits/m-p/444064#M68345</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-12T12:09:22Z</dc:date>
    </item>
  </channel>
</rss>