<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Set state getting hanged</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443879#M68300</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/joanxie"&gt;joanxie&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We observed with this wma file very easily. Removed USB while playing time is around 6 second.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With playbin2, we can't reproduce this scenario. Because we can't set state or stop while playing and it continue to play till it has data.&lt;/P&gt;&lt;P&gt;Our use case, when USB removed, we call set state to stop. That set state to stop is getting hanged for 2-3 seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using hardware audio device, so two playback can't be done simultaneously.&lt;/P&gt;&lt;P&gt;We have to stop playback as soon as USB removed, So that playback will start from previously playing device (SD/CDDA/CDROM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you have any queries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ramakrishna Kamath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jul 2015 09:18:06 GMT</pubDate>
    <dc:creator>ramakrishnakama</dc:creator>
    <dc:date>2015-07-07T09:18:06Z</dc:date>
    <item>
      <title>Set state getting hanged</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443877#M68298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Set state to stop getting hanged if we remove USB while playing attached file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once USB removed, we are trying to stop playback, But gst_element_set_state() API returning after 2-3 seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We observed aiurdemux trying to push pad buffer and which is failing continuously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our pipeline is&lt;/P&gt;&lt;P&gt;gst-launch-0.10 filesrc location=20077693327861 - Copy.wma&amp;nbsp; typefind=true ! aiurdemux name=demux demux. ! queue ! beepdec ! audioconvert ! volume ! alsasink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using gst-fsl-plugins version 3.0.8 and gstreamer version 10.36.&lt;/P&gt;&lt;P&gt;BSP version is 3.0.35 based customized BSP.&lt;/P&gt;&lt;P&gt;Board is IM6 solo based customized&amp;nbsp; board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue not reproducing with gstreamer ugly plugin asfdemux.&lt;/P&gt;&lt;P&gt;But we are facing other, many seeking related issues with asfdemux and production is very close, so we can't change to asfdemux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is very urgent, for a production program. SOP is very close.&lt;/P&gt;&lt;P&gt;Please help us analysing this ASAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards:&lt;/P&gt;&lt;P&gt;Ramakrishna Kamath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 10:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443877#M68298</guid>
      <dc:creator>ramakrishnakama</dc:creator>
      <dc:date>2015-06-30T10:53:03Z</dc:date>
    </item>
    <item>
      <title>Re: Set state getting hanged</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443878#M68299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;did you try to test other wma files? and pls try to use "gst-launch playbin2 ", and post the error log file here.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 07:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443878#M68299</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2015-07-07T07:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: Set state getting hanged</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443879#M68300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/joanxie"&gt;joanxie&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We observed with this wma file very easily. Removed USB while playing time is around 6 second.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With playbin2, we can't reproduce this scenario. Because we can't set state or stop while playing and it continue to play till it has data.&lt;/P&gt;&lt;P&gt;Our use case, when USB removed, we call set state to stop. That set state to stop is getting hanged for 2-3 seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using hardware audio device, so two playback can't be done simultaneously.&lt;/P&gt;&lt;P&gt;We have to stop playback as soon as USB removed, So that playback will start from previously playing device (SD/CDDA/CDROM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you have any queries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ramakrishna Kamath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2015 09:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-state-getting-hanged/m-p/443879#M68300</guid>
      <dc:creator>ramakrishnakama</dc:creator>
      <dc:date>2015-07-07T09:18:06Z</dc:date>
    </item>
  </channel>
</rss>