<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Error building yocto project image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443842#M68285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wayne Tsui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/#download" title="http://freescale.github.io/#download"&gt;FSL Community BSP&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2015 20:09:35 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2015-07-28T20:09:35Z</dc:date>
    <item>
      <title>Error building yocto project image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443840#M68283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;BSP: imx-3.14.28-1.0.0_ga&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 03:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443840#M68283</guid>
      <dc:creator>waynetsui</dc:creator>
      <dc:date>2015-07-24T03:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error building yocto project image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443841#M68284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;$ MACHINE=imx6dl-riotboard&amp;nbsp; source fsl-setup-release.sh -b RIoTboard -e fb &lt;/P&gt;&lt;P&gt;$ bitbake&amp;nbsp; -k core-image-minimal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021&lt;/P&gt;&lt;P&gt;Log data follows:&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_compile&lt;/P&gt;&lt;P&gt;| NOTE: make -j 3 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc&amp;nbsp; --sysroot=/home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/sysroots/imx6dl-riotboard riotboard_defconfig&lt;/P&gt;&lt;P&gt;| make: *** No rule to make target `riotboard_defconfig'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)&lt;/P&gt;&lt;P&gt;ERROR: Task 238 (/home/wayne/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'&lt;/P&gt;&lt;P&gt;WARNING: QA Issue: pulseaudio-module-console-kit rdepends on consolekit, but it isn't a build dependency? [build-deps]&lt;/P&gt;&lt;P&gt;Currently 1 running tasks (2008 of 2036):&lt;/P&gt;&lt;P&gt;0: linux-imx-3.14.28-r0 do_fetch (pid 15820)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 03:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443841#M68284</guid>
      <dc:creator>waynetsui</dc:creator>
      <dc:date>2015-07-24T03:51:33Z</dc:date>
    </item>
    <item>
      <title>Re: Error building yocto project image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443842#M68285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wayne Tsui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/#download" title="http://freescale.github.io/#download"&gt;FSL Community BSP&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 20:09:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443842#M68285</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-07-28T20:09:35Z</dc:date>
    </item>
    <item>
      <title>Re: Error building yocto project image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443843#M68286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you , gusarambula.&lt;/P&gt;&lt;H3&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 02:34:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-building-yocto-project-image/m-p/443843#M68286</guid>
      <dc:creator>waynetsui</dc:creator>
      <dc:date>2015-07-29T02:34:05Z</dc:date>
    </item>
  </channel>
</rss>