<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Play video in i.mx6 with mplayer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Play-video-in-i-mx6-with-mplayer/m-p/443384#M68201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I would like to utilize the hardware decoder in the i.mx6 to play mp4 video file using mplayer.&lt;/P&gt;&lt;P&gt;May i know what is the command to specific the mplayer to play the video using hardware decoder?&lt;/P&gt;&lt;P&gt;I tried "mplayer video.mp4", and it seems like it's playing the video using software decoder, cause the CPU usage shoot up to 100%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;ZC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Oct 2015 10:09:04 GMT</pubDate>
    <dc:creator>zc_tee</dc:creator>
    <dc:date>2015-10-08T10:09:04Z</dc:date>
    <item>
      <title>Play video in i.mx6 with mplayer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Play-video-in-i-mx6-with-mplayer/m-p/443384#M68201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I would like to utilize the hardware decoder in the i.mx6 to play mp4 video file using mplayer.&lt;/P&gt;&lt;P&gt;May i know what is the command to specific the mplayer to play the video using hardware decoder?&lt;/P&gt;&lt;P&gt;I tried "mplayer video.mp4", and it seems like it's playing the video using software decoder, cause the CPU usage shoot up to 100%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;ZC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Oct 2015 10:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Play-video-in-i-mx6-with-mplayer/m-p/443384#M68201</guid>
      <dc:creator>zc_tee</dc:creator>
      <dc:date>2015-10-08T10:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: Play video in i.mx6 with mplayer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Play-video-in-i-mx6-with-mplayer/m-p/443385#M68202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; The mplayer uses standard software codecs. Hardware options may &lt;BR /&gt; be used via gstreamer or gplay, that is based on gstreamer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 07:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Play-video-in-i-mx6-with-mplayer/m-p/443385#M68202</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-12T07:16:02Z</dc:date>
    </item>
  </channel>
</rss>