<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6DL Driver and Getting Windows 7 To Communicate As An Android Device in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Driver-and-Getting-Windows-7-To-Communicate-As-An/m-p/443359#M68198</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Kelly !&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Please try recommendations of section 3 (How do I use ADB over Ethernet?) in &lt;BR /&gt;"Android_Frequently_Asked_Questions.pdf" in android_jb4.3_1.1.0-ga documentation package :&lt;BR /&gt;---&lt;/P&gt;&lt;P&gt;From Adroid JB4.2.2, security ADB is enabled by default (ro.adb.security is set to 1). In security ADB mode, the ADB over&lt;/P&gt;&lt;P&gt;ethernet is not allowed. For more details, see How do I enable and disable security ADB?. To use the ADB over ethernet,&lt;/P&gt;&lt;P&gt;there are two steps to follow:&lt;/P&gt;&lt;P&gt;1. Disable the security ADB by changing ADB security setting in init.rc&lt;/P&gt;&lt;P&gt;2. Delete or comment the below line, and then rebuild the boot.img. setprop ro.adb.security 1.&lt;/P&gt;&lt;P&gt;3. Keep the board connecting with usb to the PC, and enable the ‘usb debuging’ from Setting-&amp;gt;Developer Options and&lt;/P&gt;&lt;P&gt;then follow the steps below to set up ADB over ethernet.&lt;/P&gt;&lt;P&gt;On the Linux PC, assuming you had built Android code or had installed Android SDK), complete the following actions to use&lt;/P&gt;&lt;P&gt;ADB over ethernet:&lt;/P&gt;&lt;P&gt;$ ping IP_OF_YOUR_BOARD (run "netcfg" on board to get IP address)&lt;/P&gt;&lt;P&gt;$ export ADBHOST=IP_OF_YOUR_BOARD&lt;/P&gt;&lt;P&gt;"adb" is a host tool created during Android build.It's under out/host/linux-x86/bin/. Make&lt;/P&gt;&lt;P&gt;sure you set path properly.&lt;/P&gt;&lt;P&gt;$ adb kill-server (Not sure why this step is needed. Just re-start adb daemon on board.)&lt;/P&gt;&lt;P&gt;$ adb shell&lt;/P&gt;&lt;P&gt;Set the ADB port properly on the device:&lt;/P&gt;&lt;P&gt;$ setprop service.adb.tcp.port 5555&lt;/P&gt;&lt;P&gt;After setting up the ADB listener port, re-enable the USB debug function in the Settings application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2015 09:37:02 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-08-18T09:37:02Z</dc:date>
    <item>
      <title>i.MX6DL Driver and Getting Windows 7 To Communicate As An Android Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Driver-and-Getting-Windows-7-To-Communicate-As-An/m-p/443358#M68197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Freescale Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;I'm trying to get my i.MX6DL device (Installed with Android OS 4.3) recognized by my host PC (Installed with Windows 7 Pro x64) as an android device and not as a generic FTDI com port.&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;I have followed the instructions carefully on this forum:&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;A href="https://community.nxp.com/thread/308981"&gt;i.MX6: Android connect to ADB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having difficulty with how to do step 6.&amp;nbsp; I went through Device Manager on my Windows machine and right-clicked on the USB port where my tablet is connected and selected "Update Driver Software".&amp;nbsp; I, then, pick from a list of drivers from my computer to select the specific file, "tetherxp.inf".&amp;nbsp; From there, I tried to get that file installed, but it comes up with this (screenshot attached) saying it needs to be x64-based systems.&amp;nbsp; Are there any updated drivers out there for i.MX6DL?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The overall goal is that I'm trying to get this i.MX6Q (installed with Android OS 4.3) to work with SmartBear, a third party test automation software, to conduct automated black-box testing.&amp;nbsp; I managed to get my Windows PC to communicate with a cheap android tablet with Lollipop Android OS installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I get my i.MX6DL device to communicate with my Windows PC?&amp;nbsp; What files/components am I missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I asked any obvious questions, sorry, I'm really new to this.&amp;nbsp; Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Kelly&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 15:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Driver-and-Getting-Windows-7-To-Communicate-As-An/m-p/443358#M68197</guid>
      <dc:creator>kellykaveny</dc:creator>
      <dc:date>2015-08-14T15:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL Driver and Getting Windows 7 To Communicate As An Android Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Driver-and-Getting-Windows-7-To-Communicate-As-An/m-p/443359#M68198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Kelly !&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Please try recommendations of section 3 (How do I use ADB over Ethernet?) in &lt;BR /&gt;"Android_Frequently_Asked_Questions.pdf" in android_jb4.3_1.1.0-ga documentation package :&lt;BR /&gt;---&lt;/P&gt;&lt;P&gt;From Adroid JB4.2.2, security ADB is enabled by default (ro.adb.security is set to 1). In security ADB mode, the ADB over&lt;/P&gt;&lt;P&gt;ethernet is not allowed. For more details, see How do I enable and disable security ADB?. To use the ADB over ethernet,&lt;/P&gt;&lt;P&gt;there are two steps to follow:&lt;/P&gt;&lt;P&gt;1. Disable the security ADB by changing ADB security setting in init.rc&lt;/P&gt;&lt;P&gt;2. Delete or comment the below line, and then rebuild the boot.img. setprop ro.adb.security 1.&lt;/P&gt;&lt;P&gt;3. Keep the board connecting with usb to the PC, and enable the ‘usb debuging’ from Setting-&amp;gt;Developer Options and&lt;/P&gt;&lt;P&gt;then follow the steps below to set up ADB over ethernet.&lt;/P&gt;&lt;P&gt;On the Linux PC, assuming you had built Android code or had installed Android SDK), complete the following actions to use&lt;/P&gt;&lt;P&gt;ADB over ethernet:&lt;/P&gt;&lt;P&gt;$ ping IP_OF_YOUR_BOARD (run "netcfg" on board to get IP address)&lt;/P&gt;&lt;P&gt;$ export ADBHOST=IP_OF_YOUR_BOARD&lt;/P&gt;&lt;P&gt;"adb" is a host tool created during Android build.It's under out/host/linux-x86/bin/. Make&lt;/P&gt;&lt;P&gt;sure you set path properly.&lt;/P&gt;&lt;P&gt;$ adb kill-server (Not sure why this step is needed. Just re-start adb daemon on board.)&lt;/P&gt;&lt;P&gt;$ adb shell&lt;/P&gt;&lt;P&gt;Set the ADB port properly on the device:&lt;/P&gt;&lt;P&gt;$ setprop service.adb.tcp.port 5555&lt;/P&gt;&lt;P&gt;After setting up the ADB listener port, re-enable the USB debug function in the Settings application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2015 09:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-Driver-and-Getting-Windows-7-To-Communicate-As-An/m-p/443359#M68198</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-18T09:37:02Z</dc:date>
    </item>
  </channel>
</rss>