<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAccessing eMMC on SabreSDB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-eMMC-on-SabreSDB/m-p/443011#M68133</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to access the eMMC on the SabreSDB board, using a low-level embedded OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can successfully detect and access both the SDCard slots (SD2 and SD3), but the same process doesn't seem to work for the eMMC... this is the first time I have worked with eMMC, so I suspect I am doing something wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the schematic, eMMC is on SD4, and two shorts SH8 and SH11 need to be shorted (I have done this)... I am wondering if that is all, or whether there are other shorts that may need to be connected or disconnected. Other than the schematic, I haven't seen any other doc. regarding the required shorts for various functions of the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions or past experiences would be greatly appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Aug 2015 02:10:42 GMT</pubDate>
    <dc:creator>adrianthewlis</dc:creator>
    <dc:date>2015-08-17T02:10:42Z</dc:date>
    <item>
      <title>Accessing eMMC on SabreSDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-eMMC-on-SabreSDB/m-p/443011#M68133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to access the eMMC on the SabreSDB board, using a low-level embedded OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can successfully detect and access both the SDCard slots (SD2 and SD3), but the same process doesn't seem to work for the eMMC... this is the first time I have worked with eMMC, so I suspect I am doing something wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the schematic, eMMC is on SD4, and two shorts SH8 and SH11 need to be shorted (I have done this)... I am wondering if that is all, or whether there are other shorts that may need to be connected or disconnected. Other than the schematic, I haven't seen any other doc. regarding the required shorts for various functions of the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions or past experiences would be greatly appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 02:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-eMMC-on-SabreSDB/m-p/443011#M68133</guid>
      <dc:creator>adrianthewlis</dc:creator>
      <dc:date>2015-08-17T02:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing eMMC on SabreSDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-eMMC-on-SabreSDB/m-p/443012#M68134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;emmc should work on Sabre board without additional modifications,&lt;/P&gt;&lt;P&gt;for emmc example one can look at SDK usdhc_mmc.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6_PLATFORM_SDK &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 03:33:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-eMMC-on-SabreSDB/m-p/443012#M68134</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-08-17T03:33:39Z</dc:date>
    </item>
  </channel>
</rss>