<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: hdmi cable connection not detected</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442781#M68073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, many thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i read that thread, but schematic of our board, for the hdmi part, is like sabreauto, so there is a voltage level shifter / protector between cpu and hdmi connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boundary seems have added a patch using RXSENSE pin to detect hdmi monitors, since they had issues with hdmi hotplug detect pin. So the hdmi lcd works at cable connection, but there is not udev event generated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So in my case, seems an hw problem, with the circuit adjusted differently, the hotplug detection start to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jul 2015 08:45:19 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2015-07-01T08:45:19Z</dc:date>
    <item>
      <title>hdmi cable connection not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442778#M68070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;using imx6q and linux 3.10.17 (boundary).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On hdmi cable connection / disconneciton, no udev event is fired.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bash-3.2# udevadm monitor&lt;/P&gt;&lt;P&gt;monitor will print the received events for:&lt;/P&gt;&lt;P&gt;UDEV - the event which udev sends out after rule processing&lt;/P&gt;&lt;P&gt;KERNEL - the kernel uevent&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am suspecting a possible hw issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bash-3.2# /lib/systemd/systemd-udevd&lt;/P&gt;&lt;P&gt;systemd-udevd[829]: starting version 208&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Every help is appreciated&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;angelo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 09:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442778#M68070</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-06-30T09:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: hdmi cable connection not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442779#M68071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seems i have some issues with the hot-plug detect pin.&lt;/P&gt;&lt;P&gt;Without any cable connected it is at 1V. With cable connected reach 2,24V, so there seems to be some pinmux configuration issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Strangely, in don't find this pin in the pinmux config map.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 12:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442779#M68071</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-06-30T12:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: hdmi cable connection not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442780#M68072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi angelo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check post on boundarydevices forum with similar issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; RooT&lt;/P&gt;&lt;P&gt;June 27, 2013 at 10:35 am..&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/" title="http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/"&gt;http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 14:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442780#M68072</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-30T14:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: hdmi cable connection not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442781#M68073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, many thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i read that thread, but schematic of our board, for the hdmi part, is like sabreauto, so there is a voltage level shifter / protector between cpu and hdmi connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boundary seems have added a patch using RXSENSE pin to detect hdmi monitors, since they had issues with hdmi hotplug detect pin. So the hdmi lcd works at cable connection, but there is not udev event generated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So in my case, seems an hw problem, with the circuit adjusted differently, the hotplug detection start to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 08:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442781#M68073</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2015-07-01T08:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: hdmi cable connection not detected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442782#M68074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi angelo&lt;/P&gt;&lt;P&gt;I have the same problem as you,if you can ,tell me how to do ,thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Sep 2018 09:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-cable-connection-not-detected/m-p/442782#M68074</guid>
      <dc:creator>zhanghaijian</dc:creator>
      <dc:date>2018-09-17T09:27:45Z</dc:date>
    </item>
  </channel>
</rss>